STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL_StatusTypeDef

Posted on June 05, 2017 at 10:04Hi,Hopefully a simple question :)Developing code on STM32F429. I have Cube installed on my Mac, running demo programs without issue.I am after the definition of HAL_StatusTypeDef . Where is it defined (what file?).I s...

Error in demostration of STM32L476RG-Nucleo

Posted on June 04, 2017 at 20:54Hi,   i have a problem compiling the Demostration of STM32L476RG-Nucleo with Adafruit LCD_1.8_SD_Joystick, the question is: 'Error retrieving content description for resource '/STM32L476RG_NUCLEO/Middlewares/FatFs/Cor...

jjros by Associate
  • 1118 Views
  • 1 replies
  • 0 kudos

STM32F401 I2C HAL Error (Possible)

Posted on June 05, 2017 at 12:57Hi,The following is based on an STM32F401 Nucleo and the IKSA101 Sensor board.  The HAL function was form anearlier version of HAL but matches that in release 1.16.0We have been working with the I2C bus on the STM32F4...

STLink: How to hold target under reset?

Posted on February 22, 2017 at 15:16How can I *hold* target connected to STLink under reset, either using CLI or GUI version of STLinkUtility, or any other software tool?ST: If there's no provision for this in STLink Utility, then please consider th...

NucleoL476RG and SD card using SPI issue

Posted on May 26, 2017 at 10:56HI Everybody,I am trying to access microSD card with NucleoL476RG board using SPI interface. I am using FatFs third party library with code (generated from stm32cubemx software). I did everything but it is not working....

Cannot compile to STM32F469I

Posted on June 03, 2017 at 16:50Hello,I try to install drivers for the above module but the widow says'no mbed microcontrollers found' I can see in the device manager'ST link debug' & 'ST link VPC ctrl' , When I connect the STM module to my PC is be...

On a system using multiple STM32F429 VI

Posted on June 05, 2017 at 08:451. We are considering a system with multiple STM32F429VI (100 pin). At that time, is it possible to connect multiple CPUs via FMC bus and flexibly access mutual FMC memory area? 2. How many nodes can the SPI multi-mas...

0690X00000607F2QAI.png

Is it possible to use Serial SRAM with the STM32F7?

Posted on June 05, 2017 at 07:27Hi all!We're working on a board that uses the STM32F7 and we'd like to add external SRAM and NOR Flash. In both cases, we'd like to use Serial memory to save on IO pins, layout, etc.In looking at the schematics for th...

STM32F3 IWDG strange behaviour

Posted on June 05, 2017 at 00:37I have implemented the IWDG on the STM32F4 and it works without problems. I have the DBG_IWDG_STOP bit in the  DBGMCU_APB1_FZ set to avoid Watchdog Faults i.e. when debugging. Did I get it right that the watchdog in a...