STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F3 IWDG strange behaviour

Posted on June 05, 2017 at 00:37I have implemented the IWDG on the STM32F4 and it works without problems. I have the DBG_IWDG_STOP bit in the  DBGMCU_APB1_FZ set to avoid Watchdog Faults i.e. when debugging. Did I get it right that the watchdog in a...

CMSIS STM32F4 setting AFR register

Posted on June 04, 2017 at 04:37There doesn't seem to be any bit definition for the GPIO AFR registers. I can set the PA5 pin alternate function to AF1 using the below code but other registers seems to have bit definitions to use. Am I missing them?...

Missing Schematic files

Posted on June 03, 2017 at 22:10I remember downloading schematic files from ST website for boards like STM32F429 Nucleao. I can't find schematic for any board now. Have they moved or taken off the website?#schematics

More Info about converting a BMP for the 746 LCD, please

Posted on June 01, 2017 at 16:26Exacly how is BSP_LCD_DrawBitmap using data?I read the text above the function definition and did just as it said. I tried various=every options, but nothing worked. I used a software called Image2Lcd(.exe).Then someo...

LMI2 by Lead
  • 2108 Views
  • 6 replies
  • 0 kudos

Demo app already installed on STM32L476-DISCO

Posted on June 03, 2017 at 08:20Hello,I fiddled around with an stm32l476 discovery board. Is there a way to reinstall the demo app originally installed on the device? Is there a place where I could find the source code?Kind regards,aannoBtw, the boa...

Reading from flash .text segment fails on STM32F427

Posted on June 02, 2017 at 17:31Hi,I am implementing a routine to verify my programmed flash image on a byte-per-byte basis against a master file on a byte-by-byte basis. I'm having problem reading from the flash at certain memory addresses. When I ...