cancel
Showing results for 
Search instead for 
Did you mean: 

Alternative SDRAM

fatih kurnaz
Associate II
Posted on December 15, 2016 at 14:53

Hi everyone, this is my first question.

I use STM32F746  and I need to interface SDRAM and this MCU. Micron SDRAM was used at the STM32F7 discovery however, at my stution this is not possible. There is any alternative to this SDRAM

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
waclawek.jan
Super User
Posted on December 15, 2016 at 16:53

SDRAMs are pretty much standardized so probably any of the will do.

Select a model and come back to talk about it.

JW

AVI-crak
Senior
Posted on December 15, 2016 at 17:27

External memory interface on the FMC may have different characteristics and price.

For very fast (maximum) operation code - SRAM memory is less than 10ns access over time, for example: IS61WV20488BLL 4 pieces. Expensive - but very quickly.

Option high volume and low cost SDRAM - 3.3V, for example MT48LC32M16A2P-75. This is for the graphics, but slowly.

Option almost free SDRAM 3.3V 128Mb. Memory for screen graphics, the cost is very low, the speed is low. QUADSPI flush memory works a little slower, but it has a low cost and high volume. Bundle of two types of memory gives acceleration and a low cost.

Posted on December 15, 2016 at 19:45

Start by constraining your search space a little. What size of SDRAM do you need? How wide of a data bus are you looking to implement? How fast does it need to be? If the factors stopping you from using the Micron part impact your choices of other parts, expand on that a little. ie price, availability, embargoed?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
fatih kurnaz
Associate II
Posted on December 26, 2016 at 12:49

I decided to use MT48LC4M32B2P-6A IT:L instead of  MT48LC4M32B2B5-6A IT:L  due to package problems. One of them speed 166mhz while other one's speed is 167mhz. Does that make any problem? 

Posted on December 26, 2016 at 12:49

I decided to use MT48LC4M32B2P-6A IT:L instead of  MT48LC4M32B2B5-6A IT:L  due to package problems. One of them speed 166mhz while other one's speed is 167mhz. Does that make any problem?