2016-12-26 3:50 AM
I use st-link tool in ubuntu,
I found that 'st-flash reset' or after I st-flash a bin file to the stm32 chip
the led action will not actually reset,
for example, after on power, the ledA will not turn on,
after I press user button ledA now is on,
but at this moment, I enter a 'st-flash reset' command, the ledA will not be off,
But if I press reset button, the ledA will be off,
I'm not sure why
Is there a command that I can reset whole chip like press reset button?
THX
2016-12-26 5:06 AM
Hi
ctc.ctc
,I recommend you to have a look toSTM32 ST-LINK utility command line interface (CLI) section on the
user manual-Nesrine-