STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Cancel a pending UART recieve

Posted on January 16, 2017 at 23:02If i start an UART receive with an interrupt looking for the next inbound byte/char;HAL_UART_Receive_IT(&huart1, &UART1_Data, 1);how can i cancel the receive before receiving the next byte/char?

How to pass a variable read in an interruption to main()

Posted on June 14, 2017 at 15:14I'm reading a serial ADC from an interruption (24 bits)I need to pass its read value to the main()I have defined in /* USER CODE BEGIN PV */ a volatile variable uint32_t  xxxxxThe xxxxx variable is right inside the in...

amelendez by Associate III
  • 5122 Views
  • 12 replies
  • 1 kudos

RBUS issue on STM32F407

Posted on June 15, 2017 at 08:40Hello.I'm working on a new board with STM32F407 MCU.Currently, there's an issue with Ethernet.After board reset, Ethernet communication is working well.But after some time (minutes or hours), the Ethernet seems to be ...

Ho Lim by Associate II
  • 1897 Views
  • 2 replies
  • 0 kudos

STM32 F7 HAL CAN bug

Posted on March 21, 2017 at 15:31We are using HAL CAN drivers for STM32 F7 (stm32f7xx_hal_can.c).During CAN tx/rx stress tests we experienced an issue resulting in CAN receive hang.The issue is due to a race condition on hcan->State variable between...

STM32F103RBT6 Error: No device found on target.

Posted on June 05, 2017 at 11:24Hello, I've designed a custom board using STM32F103RBT6. To debug the custom board I've got the STM32F103 Nucleo-64 board. As mentioned in the User manual of Nucleo 64 board(UM1724) page 18, section 6.2.4, I've connec...

STM32F7 LCD artifact

Posted on June 15, 2017 at 11:24Hi everybody, I have a custom board with STM32F777 + 800x480 TFT LCD (NHD-5.0-800480TF). The interface is RGB24 bit. LTDC color format is RGB565. Pixel clock is 25MHz.I found that some color seem to be displayed incor...

0690X00000603syQAA.jpg

UART transmitting in Interrupt mode vs. DMA mode

Posted on June 15, 2017 at 09:35Hello,I'm working with an STM32F7xx with the Cube HAL library. Im using the UART and I tried all 3 transmitting functions of UART. These are HAL_UART_Transmit, HAL_UART_Transmit_IT and HAL_UART_Transmit_DMA. all 3 met...