cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F427 CAN FD

john239955_st
Associate III
Posted on August 26, 2016 at 10:31

I am curently using the STM32F407 and F427 MicroControllers.

Can anyone advise if they are CAN FD compatible or if this is a software layer etc.

Any information would be helpful.

Rgds John W
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Posted on August 26, 2016 at 11:54

Pretty sure it is an accelerated signalling mode, and not a software layer tweak, so no I don't think this is supported by the bxCAN controller used by ST.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
john239955_st
Associate III
Posted on August 26, 2016 at 12:20

Thanks Clive.

I think CAN FD has a 8 byte to 64 byte data flexability.

Maybe  ST  support can advise on availablity.

Once again thanks for help ... and in the past.  KR John W

christoph2399
Associate II
Posted on August 30, 2016 at 10:37

for can-fd the can-controller within the silicon has to be modified. as far as i know there a some vhdl implementations for fpga's.

or you check the vendors for an external can-controler with spi interface and can-fd support.
Nesrine M_O
Lead II
Posted on January 27, 2017 at 12:22

Hi

White.John

,

The CAN FD is not supported on our current products, but it will be available on STM32H7:

https://community.st.com/0D50X00009XkihHSAR

-Nesrine-