STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! No Errorflag when writting to Write-Protected Sector

Posted on June 14, 2017 at 14:46 Hi, I'm evaluating some flash functionalities of the STM32F469NI. I have configured the Sector 12 of my STM32F469 Flash (2MB) with a Write-Protection. When I debug my Firmware I see that the corresponding bit g...

andi z by Associate II
  • 1449 Views
  • 2 replies
  • 0 kudos

Resolved! HTIM UIF clear from capture callback

Posted on June 19, 2017 at 15:26On a STM32 F777 I am configuring TIM4 to read Hall sensors (HAL_TIMEx_HallSensor_Init).I have enabled capture interrupt and in capture callback  (which is triggered at every Hall event as expected) I am clearing UIF f...

Can I program STM32F042C6T6 via STM32F0DISCOVERY?

Posted on June 20, 2017 at 08:10I am gonna use ST uM's for the first time. What I need is the simplest and cheapest PIC with CAN-BUS connectivity. So I found this: https://www.digikey.com/product-detail/en/stmicroelectronics/STM32F042C6T6/497-14648-...

Resolved! PA13 and PA14 how do i make these GPIO outputs

Posted on June 19, 2017 at 07:43I am using a custom STM32L051xxx, I want to change these two programing ports to PP outputs.I think I need to DeInit them then apply the normal Init procedure, I cand see how to DeInit these ports.ThanksKevin NZ

CubeMX Pin Speed Bug

Posted on December 01, 2016 at 17:01Hello,we are using a stm32f4 with a LTDC Display. CubeMX set's the speed of all Pins to LOW. Same problem with the MCO Pin.I hope this information will help you improve your products.Yours faithfully #!stm32-!c...

tekampe by Associate II
  • 3041 Views
  • 5 replies
  • 0 kudos

STM32F4 unwanted wakeup PA0

Posted on June 18, 2017 at 15:07Hi,Using an STM32F446.I setup PA0 to exit from standby mode.The first time I enter StandbyMode, it works well, and I can exit from standby mode by using PA0.But the next time entering standby mode, the STM32 automatic...

Kuikui by Associate III
  • 1213 Views
  • 1 replies
  • 1 kudos