STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ULPI read registers

Posted on July 07, 2017 at 14:43Hi, could you help me please to implement reading registers from USB ULPI chip ?thanks for all repliesKind regards ...

STM32CubeF4 fail clock configuration FreeRTOS projects.

Posted on July 07, 2017 at 19:35I'm trying to implement a FreeRTOS program on an STM32F429I-Disco (first rev.) using the examples in STM32CubeF4 (V1.16.0). Neither the 'Demonstration' project not the 'FreeRTOS_ThreadCreation' project will run. They ...

[Windows 10 x64] CubeMX updater deleted executable

Posted on March 20, 2017 at 08:40I tried to update STM32CubeMX yesterday to V4.20 using the built in updater (via Check Update Manager). After files were downloaded the update process started normally. Right after installation appeared to have compl...

parsec by Associate III
  • 2828 Views
  • 5 replies
  • 0 kudos

Resolved! STM32F091RC I2C DMA transfer complete

Posted on July 06, 2017 at 08:00Hello everybody,I am using I2C interface in master mode to collect data from external slave device with DMA in non-blocking mode.- HAL_I2C_Master_Transmit_DMA- HAL_I2C_Master_Receive_DMAMy program is working fine sinc...

Resolved! STM32F0 LL Library RCC Bug

Posted on July 05, 2017 at 13:52Hi,There is a bug in F0 LL library rcc module.RCC_GetSystemClockFreq() is incorrect if the mcu use HSI48 as system clock,in this case it returns HSI_VALUE but not 48MHz.

MasterPhi by Associate II
  • 1325 Views
  • 1 replies
  • 0 kudos

STM32F746ZGT6 problem with custom board [urgent]

Posted on July 04, 2017 at 21:00Dear all,   We have been developing a custom board featuring STM32F746ZGT6, and we have encountered some problems.   We are able to program the MCU using the ST-link with no problems, however, the MCU does not do anyt...

STM32F103 Shift PWM

Posted on July 06, 2017 at 18:15Dear Support,Hi,I've created two PWM with a 50% duty cycle using STM32F103 and its timer8. Now I would be grateful if you tell me how to shift one of the PWMs?#stm32f103-shift-pwm

nxp by Associate II
  • 1850 Views
  • 3 replies
  • 0 kudos

Why do not I have an overrun error? (UART + DMA)

Posted on July 06, 2017 at 11:08The problem is simple ...I am using the UART with DMA to copy 10 bytes to a memory location.Sometimes (due to some error) 11-byte packets are sent to the MCU. What happens is that the DMA will transfer the 10 bytes an...

Resolved! CubeMx 4.20.0 and oscillator problem

Posted on March 24, 2017 at 12:52I see when you change settings on RCC,  from internal oscillator to external, both line on .ioc file are setted and the code generated is this:RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORT...

Marco1 by Associate II
  • 1946 Views
  • 4 replies
  • 0 kudos