cancel
Showing results for 
Search instead for 
Did you mean: 

DMA transfer count

Andrei Chichak
Lead II
Posted on February 27, 2017 at 07:07

Since the Wish List seems to be closed, I'll put this request here.

To the processor designers:

The DMA transfer count is a 16 bit value that can be in the range 1-65535. Since 0 is a useless value and 65536 would be a useful value, could you change the hardware so that we can specify the count to be 1-65536?

You see, program FLASH on the 407 is 1MB, or 256K words. If I could specify a count of 65536, I could CRC all of program FLASH in exactly 4 transfers. 

But since the maximum is 65535, I have to either do 5 weird sized DMAs to the CRC unit, or go for 8 transfers of 32768 words each.

Just a thought.

Andrei from The Great White North

as seen on the Embedded.FM embedded systems podcast and blog.

#dma
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0