STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STSPIN32f0 - cannot generate PWM

Posted on August 28, 2017 at 13:19Hey guys! I'm trying to write custom firmware for http://www.st.com/en/motor-drivers/stspin32f0.html and I'm desperately stuck :( STSPIN32f0 is a system-in-package based on STM32F031C6. My code works fine on STM32F0...

Misha K by Associate III
  • 2041 Views
  • 3 replies
  • 1 kudos

STM32F334 HRTIM ''Half''

Posted on September 01, 2017 at 14:24Hi,Reading RM0364, Looking at 21.3.4 Timer A..E timing units stumbled upon this questionPoring over the document, Figure 243. Timer A..E overviewI wonder what the block 'Half' (between Compare1 and Period) in the...

Problem SPI STM32F405 for TLC5971

Posted on August 31, 2017 at 21:12Hi everyone,I'm trying to program ahttp://www.ti.com/product/TLC5971, with the SPI1 of STM32f405. Unfortunatly the PWM of thehttp://www.ti.com/product/TLC5971is not working. It is a LED driverI have checked the inpu...

0690X000006085mQAA.png
ignasi by Associate II
  • 2590 Views
  • 5 replies
  • 0 kudos

'OCx fast' in One-pulse mode

Posted on August 31, 2017 at 10:58I'm using STM32F429x. I'm confused by the 'OCx fast' setting when using the 'One-pulse mode' of the timer. In DM00031020 section 17.3.15, it states:In One-pulse mode, the edge detection on TIx input set the CEN bit ...

0690X000006086GQAQ.png

STM32L433R : unable to find __iar_program_start

Posted on September 01, 2017 at 07:35Hi,I am trying to figure out the initialization sequence for STM32L433R. In startup_stm32l433xx.s: i see that the vector table  first initializes the current stack pointer.After that it runs Reset_Handler. The Re...

hardik by Associate II
  • 3385 Views
  • 3 replies
  • 0 kudos

STM32L475 SPI Behaviour

Posted on September 01, 2017 at 11:26Hello,In the new design I'm working with, the STM32L475 device uses SPI interface in order to communicate with a transceiver. This transceiver is used in other designs without problems and it must act as SPI-mast...

0690X00000603mDQAQ.jpg 0690X0000060446QAA.jpg

Resolved! Where can I find specification of STM32F429I-DISC1?

Posted on September 01, 2017 at 04:23Hi,I'd like to buy STM32F429I-DISC1 kit for study. but I can't find STM32F429I-DISC1's specification what I mean is such a memory map and detail connectives information with memory map. How do I get STM32F429I-DI...

Problem when transfering Data between 2 UART Ports

Posted on September 01, 2017 at 05:07Hi,im try to transfer Data through 2 UART ports. but the problem is only the first element of the Data received.my model is like this. sent [50 1 1 52]or[50 2 2 52] through USART1 and receive it from USART3.Both ...

0690X000006085XQAQ.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.