STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L475 IRTIM Functionality

Posted on October 05, 2017 at 12:36Hello community,Even though the RM0351 mentions the availability of IRTIM, the datasheet for STM32L475 does not mention anything about it. RM0351 is for both STM32L4x5  and STM32L4x6 and STM32L476 datasheet mention...

Analog window watchdog

Posted on October 05, 2017 at 10:36Hi Guys,I have STM32L071 and I want to use analog window watchdog for detecting if voltage on channel 2 is bellow my threshold. I use it and it works really nice.I use this settings for ADC:/**Configure the global ...

0690X0000060483QAA.jpg
JAN R by Associate III
  • 1683 Views
  • 2 replies
  • 0 kudos

Selft Test Library with HAL library

Posted on October 05, 2017 at 08:20HelloI had been using old HAL Libraries from 2015 with Selt Test Library. I just upgrade my HAL library but now I am having issues with some code changes/missing functions/definitions for the Self Test Library.  Ca...

how to validate whether the stm32f4 is working in 180MHz

Posted on October 05, 2017 at 15:16Hi,We are facing  a problem, any help will be greatly appreciated.I am using stm32f446zet.  I have set to 180MHz system clock , but GPIO pin toggles at  8 MHz. We are using OPT8320 TOF sensor whose opclk runs at 24...

Remap in FMC

Posted on October 04, 2017 at 18:15Reading the reference manual of STM32F4xx (RM0090), I need some explanation about the physical remap in FMC.Page 71-72, �2.4, the interpretation of table 4 is not clear. Should I understand that when in mode Remap ...

__weak & CLANG

Posted on October 04, 2017 at 16:26Using the 5.24a Keil tool & MXCube v4.22 with V1.16 libs for F4 devicesHave a project based on mxCube and my code that works correctly :(.linking...Program Size: Code=53948 RO-data=8468 RW-data=67988 ZI-data=55308 ...

dcurran2 by Associate II
  • 2272 Views
  • 2 replies
  • 0 kudos

STM32F4 and FatFS. SD Card mounting issue.

Posted on October 04, 2017 at 11:12Simple issue description: f_mount function from FatFS causes stack problem .More detailed description:We have a project in which we use the processor STM32F407Z and we have to read files from an SD Card with using ...

Oleg M by Associate
  • 2325 Views
  • 3 replies
  • 0 kudos

stm32f205 HS Isochronous Transfer fails

Posted on October 05, 2017 at 10:41Good Morning!I am currently developing an HS USB Audio DAC using the STM32f205 microcontroller, using the HAL Library to keep things simple and to have a fast code. I have already tested my USB 'low-level-driver' b...