STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F7 - Error in final launch sequence

Posted on October 05, 2017 at 07:57Hello,I when I am about to run my application on STM32F7 discovery board, I am getting the error below.Project toolchain - SW4STM32Board - STM32F7 discovery boardThanksDheeraj#stm32f7

0690X00000608USQAY.png

I2C not work in stm32f103c8t6

Posted on October 05, 2017 at 07:58I am under test for I2C. Setting of CubeMX does not allow the pullup/down setting. The I2C device used is htu-21d (Humidity and Humidity Sensor).--source code--.. i2cTxData = (uint8_t)0xe3;    // temp while(HAL_I2C...

0690X00000608RKQAY.png 0690X00000608RLQAY.png 0690X00000608UcQAI.png

Enabling and Disabling PWM

Posted on October 05, 2017 at 04:08Hello,On an STM32F4, I've configured and can generate a  PWM signal from 2 pins, offset by 180 degrees. This is using TIM3 and TIM4, on PB5 and PB6. What I want to be able to accomplish is this. I would like to be ...

Calling stm32429I-Eval Bootloader

Posted on May 02, 2014 at 01:26Hello, we are wanting to call the built-in bootloader from our application without manipulating the BOOT0/BOOT1 pins. I am trying to use the EVAL board to validate our method. The Users Manual for the Eval board does s...

chuck2 by Associate
  • 23148 Views
  • 32 replies
  • 2 kudos

Resolved! Does STM32L072 support USB programming/debugging?

Posted on October 04, 2017 at 07:37Hello All,Is it possible that STM32L072 can be programmed/debugged through USB?  It would be nice if somebody could share reference to the possible ways the micro-controller can be programmed/debugged.Best Regards,...

sarang2 by Associate
  • 1522 Views
  • 3 replies
  • 0 kudos

Resolved! STM32L4 Demodulated Infrared Receiver Input

Posted on September 27, 2017 at 14:16Greetings community,I am developing an IR learning hardware that can transmit its learned IR codes as well. For the transmitter part, I will be using the IR_OUT pin (PA13).For the receiver part, from AN4834, I un...

STM32F030 was reconfigured by himself - help

Posted on October 03, 2017 at 13:32Hi community,I need help again. I have a problem with my stm32f030RCT6 program. Yesterday I programmed this MCU and today morning a saw problem. Problem is with reconfiguring rcc settings. MCU was programmed with P...