cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX Pin Speed Bug

tekampe
Associate II
Posted on December 01, 2016 at 17:01

Hello,

we are using a stm32f4 with a LTDC Display. CubeMX set's the speed of all Pins to LOW. Same problem with the MCO Pin.

I hope this information will help you improve your products.

Yours faithfully

#!stm32-!cubemx-!bug
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Imen.D
ST Employee
Posted on December 05, 2016 at 11:19

Dear User,

Thank you for highlighting this. Your feedback is shared internally for further review.

All comments and suggestions are welcome to improve our products.

Best Regards

-Imen-

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
LMI2
Lead
Posted on December 05, 2016 at 18:35

Speed is really rise or fall time of the pin.

Jeanne Joly
Senior III
Posted on May 04, 2017 at 17:02

Hi

Tekampe.Jens

,

Sorry for the late reply.

Yes, indeed, the maximum output speed for all LTDC pins is set to Low. And you can modify this speed to set your own speed.

You have an example in figure 39 in the

http://www.st.com/content/ccc/resource/technical/document/application_note/group0/25/ca/f9/b4/ae/fc/4e/1e/DM00287603/files/DM002876pdf/jcr:content/translations/en.DM002876pdf

. For me, here is no issue and no enhancement here to add.

If I misunderstand something, do not hesitate to reply on this post.

BR. Eric

valentin
Senior
Posted on May 04, 2017 at 22:13

Defaulting to low toggle speed is definitely the right way for CubeMX.

That reduces unnecessary high frequency contents in the signals and thus minimizes possibly unwanted EMC issues.

Posted on June 19, 2017 at 16:34

Hi

Roehrig.Valentin

‌,

generally i'm on your side, but the LCD-Displays are working at several MHz. So you have to turn it to high speed.

Or are there displays with low speed which i don't know about?

Thanks for the help.