STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Need the development board of STM32L072RB

Posted on October 06, 2017 at 12:39Hello,I need the development board of STM32L072RB. I also need the technical difference of STM32L072RB and STM32F072RB.#stm32l072rb #stm32f072rb

ketan v by Associate
  • 1158 Views
  • 2 replies
  • 0 kudos

STM32F303 internal bootloader does not work - pt. II

Posted on October 06, 2017 at 12:35Hello everybody,  I am still having problems with the STM32F303 bootloader.Description STM32F303CCExternal 24MHz CMOS oscillator1.5kohm pullup on USB_DPUSB working perfectly (in the application: no issues whatsoev...

Dma differences between stm32l4 & stm32f4

Posted on October 06, 2017 at 11:30Hello,I'm trying to port a code from stm32l4 to stm32f4 it seems that DMA initialization is a bit different between those two chips:stm32l4 requires' DMA_REQUEST_XX' : hdma_tim.Init.Request = DMA_REQUEST_4; hdma_ti...

STM32F427 conflict of USB and USART1

Posted on October 06, 2017 at 11:31Hi, everybody!I have made the multiplexer on MCU stm32f427vit6I want to use in him all 4 uart and 4 usart.Also I want to use USB_OTG_FS as the VPC console of management.But I have faced a problem if I begin to use ...

I2C/external FS PHY on USB_OTG_HS in STM32F407

Posted on June 09, 2017 at 13:31'F407's OTG_HS_GCCFG:The USB OTG HS core embeds an I2C interface allowing to connect an external FS PHY.The I2CPADEN is used to enable or disable the I2C bus connection for this interface.On which pins?Can you please ...

0690X00000607IwQAI.png

spi2 not working in stm32f070

Posted on October 04, 2017 at 07:38 Hello All currently i am working in Fatfs with stm32f070 with spi1. when i move to spi2 its not working. i am trying multiple times but i cant get success. here is my init function void SPIFlashInit(voi...

How can fix CAN Receive problem in Normal Mode

Posted on October 02, 2017 at 20:28Hi,I try to communicate via CAN. I can transmit data to PCAN but i can't receive in Normal Mode. When i use Loopback, i can receive data. Please Help me.. My configuration is here/* CAN1 init function */static void...

How to enable F746 ADC clock in CubeMX output?

Posted on October 05, 2017 at 22:59I have LCD code from Cube tool for 746 Discovery board. I have tried to get ADC working but all I get are time outs. I have tried to find differencies between my code and various adc examples and I have found some,...

LMI2 by Lead
  • 686 Views
  • 0 replies
  • 0 kudos

UART Rx of Variable Length with Interrupt

Posted on October 05, 2017 at 21:30I've seen a number of threads on there trying to find a workaround for the HAL library's inability to read a UART message of variable length. Is there any official fix to this yet, or is hacking the library still t...

Konami by Senior II
  • 946 Views
  • 1 replies
  • 0 kudos