STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to use stm32l0 comparators.

Posted on October 13, 2017 at 10:00I am using nucleo-64 board with stm32l073 microcontroller.I want to read analog data on adc pin and show the data on lcd as soon as there is change in   data on the analog pin.I want to monitor voltage  from 0-0.5 ...

Nucleo F410RB ADC dilema

Posted on October 12, 2017 at 08:50Hello,I'm newbie with STM32 microcontrollers.I want to read ADC in regular mode conversion but triggered by TIM1 Capture Compare event with a period of 100us.Despite the fact that TIM1 Capture Compare on channel 2 ...

nico 2010 by Associate II
  • 1084 Views
  • 2 replies
  • 0 kudos

Discovery board damage issue

Posted on October 13, 2017 at 07:30how many ways Discovery board(stm32f4discovery board) can be damaged? in my board LD8 is on (overflow current).how can i recognize this issue?

SD card file corruption

Posted on October 13, 2017 at 07:32HI,am using Fatfs file system in stm32f4 and writing some data in to the files which i have created , read and write operations are working fine but at some point of time when i place that sd card in windows PC am ...

STM32F4 USB OTG Enable/Disable

Posted on April 19, 2014 at 08:17Hey guys,I'm trying to disable the USBH for the F4 board after calling the ''USBH_Init'' function. Once initialized, it interferes with a connected LCD (timing issues I believe).I have tried ''USBH_DeInit'' but with ...

Resolved! HAL ADC Generic Driver - STM32Cube

Posted on October 11, 2017 at 22:16Hi,I'm very confused on how to use the HAL ADC Generic Driver. I configure the ADC using STM32Cube with all the default settings.Now I want to start the ADC and handle the interrupt. Looking into the http://www.st....

ee06091 by Associate III
  • 3475 Views
  • 4 replies
  • 0 kudos