STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Efficient way to fade a LED

Posted on October 12, 2017 at 09:36 Hi there, I'm trying to Fade (In and Out) a LED with TIM5. This is my configuration (Just a recap of the configuration): 1) Configure TIM5 in order to generate a signal with 100 Hz as period with no pulse. ...

Fede Rico by Associate III
  • 8597 Views
  • 24 replies
  • 1 kudos

get address of every register(?)

Posted on October 10, 2017 at 09:46hi.i want to get address of every register on stm32 , and set value to register but i dont  know what is address of register so how can i get the address of register?for example if i want to get address of  RCC_CFG...

STM32L476 discovery usb and example applications

Posted on July 07, 2016 at 16:38I just got on my talbe STM32L476 discovery board, but I can not find anywhere any link to download sample applications or some sample code. It looks like there is no such link on ST website. I also downloaded ST CubeM...

krestan by Associate II
  • 1787 Views
  • 2 replies
  • 0 kudos

NVIC_EnableIRQ() and kin shall handle exceptions

Posted on April 04, 2017 at 17:56According to PM0214, CMSIS functions NVIC_EnableIRQ(), NVIC_DisableIRQ(), NVIC_SetPendingIRQ(), NVIC_CleartPendingIRQ(),  NVIC_GetPendingIRQ() should support both interrupts and exceptions (of course those where this...

0690X00000606LVQAY.png

Resolved! Stm32l4 1.9.0 - FatFs naming problem

Posted on October 11, 2017 at 12:26Hi, I am using package Stm32l4 1.9.0 package on Linux with Stm32CubeMX to generate workbench project. It seems there is naming problem, since folder in downloaded repository is named 'STM32Cube_FW_L4_V1.9.0/Middlew...

How to reset slave timer in gated mode?

Posted on September 20, 2016 at 05:05How to make automatic reset of slave timer in gated mode in STM32 mcu?Summary:I've done synchronization between 2 timers: Timer#1 is configured as a slave in gated mode, Timer#2 is configured as a master, it togg...

Hard Fault interupt when erasing FLASH (intermittent)

Posted on October 12, 2017 at 16:52I frequently get a Hardfault interrupt generating when erasing (and in some cases programming) the flash using HAL_FLASHEx_Erase and HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, ..)Part is STM32L433CCIt may have...

pbayton9 by Associate III
  • 1762 Views
  • 2 replies
  • 0 kudos

Resolved! Could not 'erase sectors' for chip flash

Posted on September 18, 2017 at 04:08Hello, when I use IAP in stm32f103vct6, sometimes some of them could not 'erase sectors' , and J-link could not 'erase sectors' to these board too. But I could use 'erase chip' to these board, and then  'erase se...

Resolved! STM32CubeMX Source code format

Posted on November 15, 2015 at 16:31Hi, when CubeMX generates code, it is intended by 2 spaces. Ist there the possibility to change this behaviour to get a tab character instead. I searched in the forum and googled for a while but unfortunately, I d...

LORA network of collecting data LAN is it possible

Posted on October 10, 2017 at 14:57Hello every body , we are starting a project of a network collecting datas , we will use stm32 devices that are pretty made easy programmable with cube thans to stm!!For establishing a local network (without intern...