STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

AN2516

Posted on October 18, 2017 at 13:45Does anyone know where I can find the Simulink library or Software library that comes with AN2516 'Luenberger state observer Rotor position estimation simulink and software library'.  I found the Application Note b...

STM32H7 PLL minimum input frequency

Posted on October 18, 2017 at 11:10Hello,STM32H743 datasheet Rev. 2  in chapter 6.3.10 PLL characteristics tells 2 MHz minimum PLL input clock (f (PLL_IN)). Reference manual RM0433 Rev 3 in chapter 8.5.5 'PLL description' tells about a low frequency...

STM32F411E-Discovery PWM

Posted on October 18, 2017 at 08:36Hello.I would like to use a servo motor using STM32F411E-Discovery. Is it possible to use the pwm out mode?

HG LEE by Associate II
  • 1431 Views
  • 2 replies
  • 0 kudos

STM32F407G-DISC1 3 ADC

Posted on October 17, 2017 at 14:05Dear STM32 community,I am new at field of 32bit ARM, I have only little experience with 8bit Atmel chips and arduino programming. We need to replace expensive ADC card from National Instruments company by some chea...

Resolved! PB1 and PA1 are using the same EXT1?

Posted on October 17, 2017 at 10:45Hi.I'd like to use external interrupt PA1 nad PB1 pin.But I found the following image, I think I can't use the external interrupt PA1 and PB1. Probably I think I have to  use only one to interrupt set.Can I separat...

0690X00000608aCQAQ.png

EVALKITST7580-1 GUI problem

Posted on October 18, 2017 at 11:17Hi all,I'm using X-Nucleo-PLM01A1 with NUCLEO-F401RE and NUCLEO-L053R8 boards. I followed the guide at this link to install the EVALKITST7580-GUI and the proper firmware.https://my.st.com/content/my_st_com/en/produ...

LED don't light on Nucleo STM32F411RE

Posted on October 14, 2017 at 12:59Hi, I'm getting started with the Nucleo STM32F411RE, and the LED don't light !Here is my main.c ://*****************************************************************************////! \file main.c//! \brief main appl...

Stm32Cube MX Delete Old Firmware Files

Posted on October 17, 2017 at 14:20Hey guys,is there any way to remove old Firmware packets, which have been imported via a local stm32mcube source in cubemx.If not how can I be sure that when I start a new Project cube mx uses the latest libraries?...

edelmann by Associate II
  • 3526 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F767ZI Timer Interrupt

Posted on October 11, 2017 at 23:35Hello,I am having some difficulties wrapping my head around what's happening with my TIM3 interrupt.  I am creating a timer class for my application.  It needs a 1 microsecond resolution.  For some reason I can onl...

0690X00000608aLQAQ.png