STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Configuring I2S Clock on STM32F4?

Posted on October 11, 2017 at 00:10Hi - I'm attempting to interface a http://store.digilentinc.com/pmod-i2s-stereo-audio-output/ with my STM32F429 dev board.  The PmodI2S has a https://www.cirrus.com/products/cs4344-45-48/ DAC on it.  I'm using http...

0690X00000608YtQAI.png 0690X00000608Z3QAI.png

automotive certified STM32?

Posted on April 04, 2017 at 16:28HiI am supposed to develop a 'simple' automotive project drive some interior car lights controlled by CAN.Which ST controller is best suited for this? (Cheapest and smallest)Are any of the STM32 certified for automot...

Resolved! external clock mode problem

Posted on October 22, 2017 at 07:26Hello.I use stm32f107vct6 and use this code for external mode for timer 3  RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3 ,ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA|RCC_APB2Periph_AFIO, ENABLE);GPIO_InitType...

STM32F103 Uart 921600 System Hangup

Posted on October 20, 2017 at 17:33I am using STM32F103ZF with Keil RTX RTOS on it. I have a UART configured at 921600 baud. I am sending about 2000 bytes a second and receive about 200 bytes every 5 second. What I am observing is I can transmit fin...

STM32F4 SPI DMA Unexpected Overrun Error

Posted on October 17, 2017 at 01:30Hi everyone!I'm working with an external IC which must be read with a 'burst transfer'.I have to receive 122 half words (16 bit spi transfers), so I use an SPI DMA reception.When I configure a buffer in my code as ...

RTC cause main code stop working

Posted on October 21, 2017 at 01:06I was running RTC with stm32f051. I use cmsis and using LSE(32.768 khz) for rtc.I use this code for setup rtc with alarm . when interrupt of rtc is running the other section of code stop working but the interrupt r...

STM32F4 DMA REQ and ACK for External DMA

Posted on October 21, 2017 at 02:13I'm trying to interface my STM32F407 MCU with a peripheral device that has independent DMA/MPU interfaces. The MPU interface is available in two modes (68 and 80) and the data bus width is available in 8-bit and 16...

Zaher by Senior II
  • 1605 Views
  • 2 replies
  • 0 kudos