cancel
Showing results for 
Search instead for 
Did you mean: 

HAL_UART_Transmit_IT(); Issue

Manojkumar Subramaniam
Associate II
Posted on July 03, 2017 at 00:53

Hello everybody, I just got into STM32 development and using the HAL library primarily for my developments now. I am having a issue with UART IT library function. Why when I have a for loop delay or HAL_Delay in my main code the Buffer data is not updated, I keep receiving the first byte consecutively, it worked very well if I don't have delays in my code.

main raw code :

https://github.com/manoj153/Fingerprint_Netrikkan/tree/UARTSWAPTEST/Src

Keil MDK project :

https://github.com/manoj153/Fingerprint_Netrikkan/tree/UARTSWAPTEST/MDK-ARM

 

Or if you want to clone the repo : 

https://github.com/manoj153/Fingerprint_Netrikkan/tree/UARTSWAPTEST

 

Board : STM

http://www.st.com/en/evaluation-tools/32f746gdiscovery.html

Thank You, 

Looking forward for a solution from the experts from the community  

#uart-it #stm32 #keep-receiving-the-first-char #stm3247
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0