cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F469 and DSI

michael239955
Associate III
Posted on June 06, 2017 at 01:03

We are using an STM32F469 in our design. We also utilize the device's DSI interface to a 400X400 LCD (round). We are clocking the micro with a 16MHZ crystal and producing a SYSCLK of 180MHZ. All is good. Now, I am slowing down the SYSCLOCK to 90MHZ to save some power, but in doing so our display gets messed up. The image on the screen is shifted by 50%. Meaning the visible image has walked 200 pixels to the right and wraps back around. How does changing the SYSCLK have this effect?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee

Posted on June 09, 2017 at 15:41

Hi Carrier.Michael‌,

I think that the AN4861 may bring you some explanation for the issue and help to fix it.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.