STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hi, i want drivers for stm32l476mcu

Posted on November 01, 2017 at 10:38Hi,I bought stm32l476 micro controller. I want drivers for this board(stm32l476).please send me the link where i can get those drivers.Regards,Ashok

stm32f205 USB and new project questions.

Posted on November 01, 2017 at 08:48Good morningStm32F205RBT We are planning a new project to control with MCU.I'll use the LCD,Use the six buttons (Enter, esc, left, right, up, down) to set the timeEach IO will be recorded in the flash ROM when the...

How to synchronize DAC, ADC together?

Posted on October 31, 2017 at 07:13I am using stm32L476 discovery board. I am trying to generate triangular wave with DAC. I am using two lookup tables for the DAC(1 for each up slope and down slope). I am giving sine wave at ADC input and I am gett...

C S by Associate II
  • 2299 Views
  • 2 replies
  • 0 kudos

stm32f373 adc ftrig

Posted on October 30, 2017 at 05:13Hi,Looking at the other stm32 MCU's like the stm32f407 I see in their datasheet a spec fTRIG (aka the External trigger frequency) ... however I cannot see the same spec for the 16bit SDADC on the stm32f373 datashee...

othane by Associate II
  • 1665 Views
  • 3 replies
  • 0 kudos

STM32F3Discovery Project in Ac6/OpenSTM32

Posted on October 31, 2017 at 23:30Hi forum,I have downloaded the STM32F3Discovery Demo Source Project.There are project files for several IDEs included but looks like none for Ac6/OpenSTM32.Has somebody converted that already?

STM32CubeMX project reuse

Posted on September 26, 2017 at 17:56If I have .ioc project for a UFBGA176 and then I want to migrate to an LQFP144, is there a way to proceed with STM32CubeMX without loosing all the work in 'Configuration' tab?In other words is there a way to sepa...

LRWAN_V1.1.1 example PA0 and PA4

Posted on October 30, 2017 at 10:26Hi,I am using the B-L072Z-LRWAN1 board running the End-Node example.I added 4 GPIO external interrupts on PA0,PA2,PA3 and PA4.Before the the board goes into Stop Mode all 4 intterupts works as expected.//----PA0, P...

how can i use LCD 4*20 in IAR with CMSIS?

Posted on October 30, 2017 at 09:18hi.i want to use LCD 4*20 in IAR with CMSIS  , but i didn't found any library for this.and if i dont want to write a library for lcd , what do i do ?where do i can found this library?or shall i write this library?o...

tim3 rises all interrupt flags even though it shouldn't

Posted on October 31, 2017 at 11:46Hello, I have timer 3 setup like this:ARR = 8400PSC = 99CCR1 = 4200CCR2-4 = 0xFFFFCR1.CEN = 1DIER.CC1IE = 1DIER.UIE = 1when i run my code after one interrupt all interrupt flags get set to 1, obviously this shouldn...