cancel
Showing results for 
Search instead for 
Did you mean: 

Printf to debug viewer(in Keil) on Cortex M0

hospodar
Associate III
Posted on January 02, 2013 at 23:20

Hello,

do STM32F0 support function, where printf output is forwarded to ''Debug (printf) Viewer'' in Keil not to UART?

Thanks

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Posted on January 03, 2013 at 02:32

Trace (ETM, ITM, DWT) not available on Cortex-M0

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Bob Boys
Senior
Posted on June 30, 2017 at 18:13

This is possible using uVision Event Recorder:

See

https://community.st.com/0D50X00009XkeHKSAZ

 

Bob Boys

ARM

Posted on June 30, 2017 at 18:46

The IDE can do it for you - go to 'Manage Run-Time Environment' and select the right option for STDOUT. In this case ITM.

0690X00000607ZhQAI.png
Posted on June 30, 2017 at 18:47

For sure for non M0 devices  - in this case not available on F0.

Bob Boys
Senior
Posted on July 01, 2017 at 04:17

Hello

The 'USER' selection is normally used to redirect to hardware such as a UART.

Using ITM or EVR does not require a UART or other user hardware.

Attached is an updated version of the Keil ST-Link appnote. I will put this on Keil.com early next week:

See page 15 for the method to provide printf for STM32F0 Coretx-M0 processors. This will also work for other Cortex-M devices.

Bob Boys

________________

Attachments :

StLink_3.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyV0&d=%2Fa%2F0X0000000b9l%2FCZUhXcxo1Z.qMFD1lt5rT1NXY4zT1WG81B3GSWYdXcU&asPdf=false