STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Memory requirements for FFT

Posted on November 14, 2017 at 04:36Dear All,I'd like to implement FFT within STM32F103C8 without any extra memory buffers.So I want to know how many memories are needed to implement if I have 2592x1944x8bit size's one image?

STM32 n-Pulse Generation

Posted on January 11, 2017 at 15:21I am trying to interface a Teknic Clearpath SDSK motor to STM32F7 Nucleo Dev Board. It is a Brushless DC motor with a stepper like interface. The motor moves a set distance based on the number of pulses it receives...

Neo M by Associate II
  • 5686 Views
  • 6 replies
  • 0 kudos

Cube Project/Demo similar to the F4 Demo Builder

Posted on November 12, 2017 at 01:01Hello Folk!I checked all the demos, projects, templates, whatever, inside the Cube package for F4 devices but couldn't find anything similar to the F4 demo builder package. Audio playback layer in particular. Asid...

Zaher by Senior II
  • 1328 Views
  • 2 replies
  • 0 kudos

STM32L0 How do i disconnect the SW-DB once connected

Posted on October 31, 2017 at 04:53Hi, I am using an STM32L053xx in StandBy mode for 500ms and Run mode for 2ms.  I have noticed in StandBy my PCB draws about 120u amps more after the SW-DB has been connected.To correct this I need to disconnect the...

STM32 USB VCP problem under Windows 10

Posted on November 14, 2017 at 01:25Hi,i use STM32F107RB in my project wherein is an USB VCP virtual com port driver (The basic of the USB VCP is the STM3210C-EVAL_USB_decice_VCP example of the Atollic True Studio). It works well if i use under Wind...

STM32L486 VREFBUF precision

Posted on November 13, 2017 at 09:42We have build some prototypes of  a new product containing the STM32L486 (UFBGA132 package). The VREF+ pin is buffered with 1µF and 100nF. I measured the reference voltage with two different calibrated multimeter...

When to set TIM1 pwm channels - 3phase drive

Posted on November 13, 2017 at 20:52Hello,I have a  project where a 3phase DC BLDC motor is required to be spined.For now i have : - 3 hall sensors conected to CH1,2,3 of the TIMER2.                          - 6 complementary pwms via Timer1In the T...

Bogdan by Senior
  • 713 Views
  • 0 replies
  • 0 kudos