STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Understanding SysTick_Handler()

Posted on August 28, 2017 at 13:46Hello everyone,I am setting up a project to make some tests with an STM32F7 MCU. I am using the STM32Cube HAL and the idea is to configure some timers and their interrupts using this HAL. The board is equipped with ...

Quick start STM32F7

Posted on November 14, 2017 at 16:491. I have necessity force to start STM32F7 after reset as fast as possible.How to do it correctly using HAL or Low-layer drivers?In 'Description of STM32F7 HAL and Low-layer drivers' I find in chapter 'FAQs'Follow...

creating bootloader for sensor tile

Posted on September 29, 2017 at 21:33I am using the ST SensorTile for development.  Now trying to understand the OTA and Bootloader.Currently only able to find the binary for bootloader.Does ST provide source code / project to build our own bootload...

Resolved! Please Correct BUG with SD code generation

Posted on March 02, 2017 at 18:57The new format of code generation makes a BUG in the file: bsp_driver_sd.hThe BUG prevent building FAT_FS modulesTo solve the issue line 67 should be changed with the following ones:&sharpifndef BSP_SD_CardInfo  &sha...

Have you come across UNI/O source code for STM32?

Posted on July 01, 2015 at 15:48I am working with the STM32F407 microcontroller and I need to interface to a one-wire serial flash memory from Microchip using their UNI/O protocol (https://en.wikipedia.org/wiki/UNI/O). I am new to ST microcontroller...

arnold_w by Senior II
  • 1307 Views
  • 1 replies
  • 0 kudos

Batch unique ID programming

Posted on November 14, 2017 at 13:19Hi,I have 100 units that I need to program with unique ID, SN... somewhere in the FLASH memoryWhat is the easiest way to do it?Thx,Michael

priven by Associate II
  • 1217 Views
  • 3 replies
  • 0 kudos

SPI3 Chip Select (NSS) not working

Posted on November 14, 2017 at 10:47 Hello there, with my STM32F103, I'm working with the M25P40 SPI flash memory. With cube32Mx I configured the SPI3 with Chip Select (NSS) hardware and I perform Read/Write/WriteRead operation with Interru...

0690X0000060PDqQAM.png
Fede Rico by Associate III
  • 2485 Views
  • 4 replies
  • 0 kudos

stm32f469i-discovery case/enclosure

Posted on November 14, 2017 at 14:30I have recently completed a project to write a password manager using the stm32f469i-discovery board and would now like to take it on the road with me but am having a problem finding a suitable enclosure to protec...