cancel
Showing results for 
Search instead for 
Did you mean: 

B-L072Z-LRWAN1, CubeMX project

Jin ho An
Associate II
Posted on August 23, 2017 at 11:11

Hi.

I am analyzing with B-L072Z-LRWAN1.

If you have a CubeMX project file, it will help you analyze it.

Can not convert AT_Slave project to CubeMX project?

Clock, and LPUART settings.

Please.
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on August 23, 2017 at 14:07

You will need to merge/refactor the code at a HAL level

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on August 24, 2017 at 04:39

Thank you for your reply.

Can I make 'End Code' instead of 'AT_Slave'?
Posted on August 24, 2017 at 05:28

Not sure exactly what that is, but most use cases that I see and discuss with people are ones using the L072Z as the sole micro-controller in the design, and it doesn't need to talk in AT commands to itself. So the AT command layer is stripped out, and you just call the underlying functions directly to achieve the desired connectivity.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..