STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L4 and F1 RTC Alarm HAL libraries

Posted on December 22, 2017 at 12:26Hi,HAL libraries are used to make easy project porting from a series or MCU to another one ...I just found a trouble, i used RTC ALARM in L4 and L0 MCU and set a fixed time to make alarm each 24 hours. it works wi...

mbedTLS Client ssl handshake failed

Posted on December 22, 2017 at 11:45I am using STM32F769I-DISCO. and using STM32Cube_FW_F7_V1.8.0I want to test mbedTLS SSL_Client example.I am using STM32Cube_FW_F7_V1.8.0\Utilities\PC_Software\ssl_server\ssl_server.exe as SSL server in Windows 7.W...

ritesh by Associate II
  • 1657 Views
  • 0 replies
  • 0 kudos

Problem with Flash loader demonstrator on STM32L452RE

Posted on October 18, 2017 at 14:35Hello,I'm trying to use the flash loader demonstartor change the software on my STM32L452RE.I place my device in bootloader mode, and I manage to connect using Flash Loader demonstrator, but then I'm on a page aski...

Resolved! CubeMX generator have a problems

Posted on December 20, 2017 at 18:21Hello guys! Help me please... I have problems with the CubeMX, can not generator code create project((( Operating system Linux Mint 18

Hosting by Associate III
  • 1970 Views
  • 4 replies
  • 0 kudos

STM32L4R9-EVAL UART Promblem

Posted on December 19, 2017 at 12:48Hello, I'm struggling to make (any of) the UART examples for the STM32L4R9-EVAL board work, so far without any success. Has any one here was able to get any data from the UART port (through the ST_Link interface) ...

Resolved! STM32L432KC - Timer DMA Triggering ADC DMA?

Posted on February 17, 2017 at 05:19 Hi, On my larger project, I would like to be able to generate a timer that will trigger an ADC read on each rising edge. I was able to tackle this problem by creating a smaller project and executing it! Sup...

Nolan L by Associate III
  • 7162 Views
  • 7 replies
  • 0 kudos

Where is STM32 RTC counter value? (Not F1 family)

Posted on December 08, 2016 at 20:29Hi,In the scheduling system we use we need a simple 32kHz low power counter value. Exactly like in the stm32F1 family is present.But in any other family, the RTC registers are replaced by Time and Date registers.I...

Resolved! STM32l4 in stop2 mode with rtc alarm

Posted on December 21, 2017 at 07:47Dear all i want to wakeup stm32l4 in every two minute from stop2 mode using RTC,give me suggestion.I am using example code from st and trying  PWR_STOP2_RTC on my custom board,i am finding that l4 is not going in ...

Receive UART WWDG_IRQHandler infinite loop

Posted on December 21, 2017 at 14:25Good morning. I'v tried to perform an UART receive on stm32f407vg board using RXNE interrupt. But when i execute the code it is blocked on WWDG_IRQHandler infinite loop. I post my code:#include 'stm32f4xx.h'#inclu...

Resolved! Toggling GPIO STM32F407VGT6

Posted on December 19, 2017 at 05:50Hello,I am using the Mikro Pro C IDE to write a simple program to toggle GPIOA pin 0 on a STM32F407VGT6. When I compile I get several errors, but I don't think it has to do with an error in my code, more or less a...

0690X00000609FsQAI.png