STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

internal flash

Posted on February 19, 2018 at 09:57 hello! i am working with stm32 cortex-M0? IN FACT i want to know how to modify bytes from the internal flash without erasing the whole page , in addition i don't have RAM space to copy code there and modify byte...

ham10za by Associate II
  • 9266 Views
  • 29 replies
  • 0 kudos

Resolved! STM32CubeMX for STM32L4 Discovery kit IoT node

Posted on September 19, 2017 at 04:17Hi,I would like to generate the code by using STM32CubeMX for STM32L4 Discovery kit IoT node (B-L475E-IOT01A).But I don't see the STM32L4 Discovery kit IoT node in the Boards List.Could you suggest for me?Thank y...

Good B by Associate II
  • 1313 Views
  • 2 replies
  • 0 kudos

STM systick counter

Posted on July 31, 2012 at 06:55I am trying to use systick counter to verify the accuracy of my RTC. Bascially what I did is check the systick counter against RTC timer in the second interrupt. I find it seems the systick count is heavily affected b...

leon23 by Associate II
  • 5080 Views
  • 3 replies
  • 0 kudos

Systick and TIM6

Posted on February 19, 2018 at 12:55The original post was too long to process during our migration. Please click on the attachment to read the original post.

AutoPolling QSPI and memory erase

Posted on February 16, 2018 at 19:52Hello friends.I have a problem. I erase external memory. But this procedure last long time. So I set autopolling mode with interrupt. But It doesn't work.When I send erase command I need wait on WIP bit in status ...

0690X00000609i6QAA.png

Encoder overflow or underflow?

Posted on February 17, 2018 at 16:56Hello,I configured the TIMER1 to use like an encoder counter. My question is: How I can detect inside the in the interrupt function if the interrupt was caused by an overflow or underflow in the counter?void HAL_T...

Raül G by Associate II
  • 4954 Views
  • 5 replies
  • 0 kudos

Setting nss_soft in Master (SPI)

Posted on February 17, 2018 at 23:00I want to set NSS pin to software mode in master using STM32F103RB. But I've few questions?In reference manual, they say,In NSS Software mode, set the SSM and SSI bits in the SPI_CR1 register. If the NSS pin is re...

CAN Filter passes more messages as defined

Posted on February 17, 2018 at 10:09 I have a problem with STM32F042 CAN Filter mechanism. Basically the CAN is working. I can send and receive messages. But my filter are passing more messages to the FIFO as defined. This is leading to an overru...

klaus2 by Associate II
  • 1371 Views
  • 3 replies
  • 0 kudos

stm32F4xx - UART - IT - stay enable!

Posted on February 19, 2018 at 09:51hi,stm32F4xx configured with 2 uart(uart1 and uart2) with DMA and uart (UART_IT_IDLE).Sometime, i have a issue regarding the status of uart2 IT stay enable.when i receive message on uart2, fct HAL_UART_IdleCallbac...

Resolved! STM32 FW_F7_V1.3.1 I2C HAL_I2C_Master_Receive() BUG

Posted on May 18, 2016 at 14:18 i tried to port software from F4 to F7 but got HAL_TIMEOUT and wrong reading of data from functio n HAL_I2C_Master_Receive() i changed the following code --- stm32f7xx_hal_i2c.c Tue Dec 22 14:36:08 2...