cancel
Showing results for 
Search instead for 
Did you mean: 

hi,i have nucleo-l476rg board.i want to know,if i can use on-board st-link of nucleo to flash other stm boards,apart from nucleo

kalpana lopinti
Associate II
Posted on January 09, 2018 at 06:23

we have st-link come along with nucleo boards.i want to use same st-link to flash custom stm-boards llike we do with external st-link.is it possible?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on January 09, 2018 at 06:42

http://www.st.com/content/ccc/resource/technical/document/user_manual/98/2e/fa/4b/e0/82/43/b7/DM00105823.pdf/files/DM00105823.pdf/jcr:content/translations/en.DM00105823.pdf

 

chapter 6.2.4

It is very easy to use the ST-LINK/V2-1 to program the STM32 on an external application.

Simply remove the two jumpers from CN2 as illustrated in Figure9: Using ST-LINK/V2-1 to program the STM32 on an external application

, and connect the application to the CN4 debug connector according to Ta b l e 5