Question
run motor without the use of st motor control workbench
Posted on January 08, 2018 at 16:08
Hi, I am trying to modify the the code which is compiled from st motor control workbench. So far i have successfully run using st motor control workbench. May I ask is it possible to modify the code so that it does not need to run through the st motor control workbench which include adjusting the speed of motor just by varying the potential-meter on motor driver. If it is possible, which document do I need to refer to? Thanks