STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Broken Project from cube v 4.24.0

Posted on January 31, 2018 at 01:46so, i've updated cube to v4.24.0and it starts to make broken .ioc filesi tried several ways to reproduce same issue and here's the problem.1. make a project with stm32f407ze ( not sure it's because of this but.. )2...

STM32F030 TIM16_CH1N and TIM17_CH1N input capture not work

Posted on February 20, 2018 at 10:30Hi,I have configure the TIM16_CH1N and TIM17_CH1N timers as input capture to PB6 and PB7 pin respectively:uint8_t Tim16_17_Init ( void ){    GPIO_InitTypeDef GPIO_InitStructure;    NVIC_InitTypeDef NVIC_InitStruct...

u23 by Senior
  • 2153 Views
  • 3 replies
  • 0 kudos

Resolved! CubeMX 4.24 migrate problem

Posted on January 25, 2018 at 05:11OS: Win10ico version : 4.23 / FW_F4 V1.18.0I can't migrate my project from 4.23 to 4.24. Attach is my ico file.Thank you.

liu yong by Associate II
  • 2487 Views
  • 6 replies
  • 0 kudos

Resolved! CubeMX CAN Config Fails in 4.24

Posted on January 27, 2018 at 08:21Using an STM32L4xx MCU in CubeMX. Enable the CAN peripheral. Go to configuration and click CAN1 ->You'll notice that no dialog box ever appears.Same with migrating an STM32L4xx based project to the new 1.11 framewo...

0690X00000609THQAY.png

Resolved! SMT32F7; FMC with SDRAM & NAND Problem.

Posted on February 16, 2018 at 15:53I have a problem with an STM32F767 on a custom board with SDRAM and NAND SLC memory connected to the FMC.The NAND is 8 bit, the SDRAM is 32bit, so only the [D0:D7] signals are shared between the SDRAM and the NAND...

, IAP in stm32f429 (custom board and firmware)

Posted on February 19, 2018 at 12:45I am writing a custom firmware for a stf32m429 MCU. I need about 128Kbytes of EEprom but the ECU has none. Due to security reasons I cannot use external eeprom chips. I was wondering if the following scenario is f...

STM32F373R8 CANBUS Communication

Posted on February 21, 2018 at 06:09The original post was too long to process during our migration. Please click on the attachment to read the original post.