STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ETM trace with Ulink pro in STM32CUBEMX

Posted on March 03, 2018 at 16:10I am using STM3210C EVAL board (stm32f107vc). UlinkPro debugger.Here is the tutorial I found from keil.com. http://www.keil.com/support/man/docs/ulinkpro/ulinkpro_stm32f10xxx_etm.htm Here is the snipping.So, when we ...

0690X00000609t0QAA.png 0690X00000609t4QAA.png

Resolved! STM32L431VCT6 USART as UART port configuration

Posted on March 01, 2018 at 12:31Hi How can we use USART as UART port in STM32L431VCT6 micro controllerI am looking for connecting two STM32L4 micro controller with TX, RX and Ground lines.Already UART port is being used for other purpose and have o...

Low power operation for STM32L4xx devices

Posted on March 03, 2018 at 01:22This is for shutdown power consumption.Table 5 of AN4621 says '8 nA w/o RTC' and '260 nA w/ RTC'Table 37 in STM32L443xC datasheet - en.DM00254865.pdf (July 2017) says 8nA and 25nA for the same conditions.Something fe...

Mikexx by Associate II
  • 1140 Views
  • 2 replies
  • 0 kudos

STM32F407 and UlinkPro D

Posted on March 15, 2017 at 17:45Hello!I want to program/debug an STM32F407 using the UlinkPro D. I have connected the Ulink to STM32 using datasheet for the micro controller and found what I think is the correct pinout for the Ulink.Serial Wire Deb...

higher baudrate than 115200 in irda mode possible ?

Posted on March 03, 2018 at 21:03Hi, I am using two STM32L452 nucleo boards to communicate over irda transceivers. One board only as transmitter and one  only as receiver. The datasheet of the stm32 contains a value of 115200 as maximum baudrate whe...