STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Running STM32F4 Discovery board on 1.8 Volt

Posted on March 03, 2018 at 21:15I need to run the board on 1.8 v.I found https://www.eevblog.com/forum/microcontrollers/using-stm32f4-discovery-board-on-1-8-volt/ thread about the changes need to be made to the board. However, it is not clear to me...

Mostafa B by Associate II
  • 1814 Views
  • 4 replies
  • 0 kudos

Editing IAR .o file

Posted on March 04, 2018 at 15:26Hi ST,I'm using STM32F767 processor.Because of the need of our project,I meet a problem that I don't know how to editing .icf file of STM32F767 in IAR project.What should I do?And how I should do to add the .o file i...

ETM trace with Ulink pro in STM32CUBEMX

Posted on March 03, 2018 at 16:10I am using STM3210C EVAL board (stm32f107vc). UlinkPro debugger.Here is the tutorial I found from keil.com. http://www.keil.com/support/man/docs/ulinkpro/ulinkpro_stm32f10xxx_etm.htm Here is the snipping.So, when we ...

0690X00000609t0QAA.png 0690X00000609t4QAA.png

Resolved! STM32L431VCT6 USART as UART port configuration

Posted on March 01, 2018 at 12:31Hi How can we use USART as UART port in STM32L431VCT6 micro controllerI am looking for connecting two STM32L4 micro controller with TX, RX and Ground lines.Already UART port is being used for other purpose and have o...

Low power operation for STM32L4xx devices

Posted on March 03, 2018 at 01:22This is for shutdown power consumption.Table 5 of AN4621 says '8 nA w/o RTC' and '260 nA w/ RTC'Table 37 in STM32L443xC datasheet - en.DM00254865.pdf (July 2017) says 8nA and 25nA for the same conditions.Something fe...

Mikexx by Associate II
  • 1125 Views
  • 2 replies
  • 0 kudos