cancel
Showing results for 
Search instead for 
Did you mean: 

KEIL debug issues with STM32F030F4P6

Vu.Andy
Associate III
Posted on November 02, 2017 at 22:28

I am having some debugging issues with Keil uVision5 eval (free) version. Now the STM32F030F4P6 has 16K bytes, and when I compile my program, it is approaching the memory limits. Below is the code size:

Program Size: Code=15524 RO-data=300 RW-data=540 ZI-data=2460

Here is my specific problem. I have two functions:

double GetSingleCellVolt(int cell);

void GetCellVoltArray(double *pa_volt)

{

call GetSingleCellVolt(int cell);

}

Now when I call GetCellVoltArray() by itself, then it always returns 0 regardless.

But if I call GetCellVoltArray() which calls GetSingleCellVolt(), then it works fine.

Now when I step inside the function GetSingleCellVolt(), to debug, the codes seem

to be executed in wrong order. For example, line 4 gets executed before line 3 ....

And there are variables inside GetSingleCellVolt() cannot be viewed because the

debugger complains that the variable is 'not in scope' but clearly the variables are

inside the function.

I don't know if this problem is specific to my case since my guess is my memory

limit is right up to the uC limit or it's something else.

Thanks.

Note: this post was migrated and contained many threaded conversations, some content may be missing.
This discussion is locked. Please start a new topic to ask your question.
25 REPLIES 25
Posted on November 02, 2017 at 23:13

If execution order is confusing try turning off optimization, one C line may take multiple assembler lines, and those may be rearranged.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Andrew Neil
Super User
Posted on November 02, 2017 at 23:13

The code you posted doesn't make sense:

double GetSingleCellVolt(int cell);
void GetCellVoltArray(double *pa_volt)
{
 call GetSingleCellVolt(int cell);
}�?�?�?�?�?

That wouldn't even compile!

Please copy & past the actual code - and use the 'Syntax highlighter' to get properly spaced code layout - as above

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Posted on November 02, 2017 at 23:52

Could you point out which 'optimization' should be turned off?  There is an optimization level 'Level 1 'O1', Level 2 ...

I set 'Optimzation' to default but I am having the same issue where codes are executed not in order and some lines of codes are skipped.

For example, these codes are used to read voltage using I2C:

    int val = 0;

    uint8_t b[4];

      int cellidx = ar_mainCellV_idx[(int)2];

    b[0] = (uint8_t)((0x0c + (cellidx)*2));

    ReadBuffer(G_BQ76930Addr, b, 2);

 

    val = b[0] << 8;

    val = val | b[1];

    double cell_volt =  (double)val * G_cell_volt_lsb;

   The debugger executes ReadBuffer(G_BQ76930Addr, b, 2) then b[0] = (uint8_t)((0x0c + (cellidx)*2))

   then it would skip the next three lines altogether.  I mean these are just basic codes so I am not sure

what could be the problem.

I am using the 'free' version so could it be the case?

Thanks.

Posted on November 03, 2017 at 00:02

Level 0 would be what you want.

http://www.keil.com/support/man/docs/uv4/uv4_dg_adscc.htm

 

You might also want to look at the assembler code generated and how that meshes with source.

Sometimes it helps to print out intermediate values, and makes sure things proceed as expected and have appropriate values.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on November 03, 2017 at 00:23

Thank you.  Setting 'Optimization' to Level 0 seems to be working at the moment.  But I am having a bit of doubt as to the stability of the 'free' version.

I've been using this same 'free' version before for I2C stuffs but never had this problem before.  I am not sure why I would have this problem now.

Thanks.

Posted on November 03, 2017 at 00:32

I don't think the free version is materially different from stock. The CM0 is however a significantly weaker core, with stripped down features including the ITM/DWT

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on November 03, 2017 at 00:34

Well I guess I am not trying to do any thing fancy but just some basic debugging can't seem to work.  Now I am having another strange problem.  At start up of debugging, it stucks in a endless loops.  Now it won't go to main().

ApplicationStart

                 LDR     R0, =SystemInit

                 BLX     R0

                 LDR     R0, =__main

                 BX      R0

                 ENDP
Posted on November 03, 2017 at 00:42

Check what you are doing in SystemInit() likely in system_stm32l0xx.c. Look for loops waiting for clock sources, or PLL, etc.

__main is Keil's runtime initialization code that copies or zeros the statics in RAM before calling your main() function.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on November 03, 2017 at 11:13

for some reason, that got stuck in moderation for over 12 hours!

:(

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.