cancel
Showing results for 
Search instead for 
Did you mean: 

How to distinguish L073 vs L072; L053 vs L052; etc, at run time?

Andrew Neil
Super User
Posted on October 31, 2017 at 20:16

The RM0367 (

STM32L0x3)

and RM0376 (

STM32L0x2)

say

The ... products integrate an MCU ID code. This ID identifies the ST MCU part number (sic) and the die revision.

But that is

not

true!

The Device IDs are the same for both STM32L0x3 parts and STM32L0x2 parts! 

In fact, the Device ID just tells you whether it is a Cat-3 or Cat-5 device:

Both L073 and L072 are Cat-5 devices - both have Device ID 447;

Both L053 and L052 are Cat-3 devices - both have Device ID 417.

So: how can these device pairs be distinguished at run time?

The only difference seems to be the presence of the LCD controller on L0x3 (absent on L0x2) - so is there a way to detect the presence/absence of the LCD controller?

#st32l053 #st32l052 #mcu-id #dbg_idcode #device-id #l073 #lo72 #l053 #l052
A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on October 31, 2017 at 21:57

Could try setting the bits in the clock enable registers high/low and see which bits are sticky.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..