STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! wake up from stop mode using I2C

Posted on March 15, 2018 at 14:05Hi everybody,i'm using STM32L051T6 MCU and i need to wake up from stop mode using I2Ci've read the last datasheet version and it is possible but there is an errata sheet that reports thati it is impossible.The datash...

Measuremet of internal temperature on ST32F303RCT6

Posted on March 13, 2018 at 18:46We have been using processor temperature measurement for a long time with different families of STM32: M3, F3, F4. Only the processor STM32F303RCT6 does not work. The measured voltage of the sensor is 2.22V and is re...

milan23 by Associate II
  • 3256 Views
  • 6 replies
  • 0 kudos

Resolved! stm32f071 - Port PD2 not configurable as output

Posted on March 15, 2018 at 18:34Dear everybody,in my code, i am not able to set my Port PD2 as output.As can be seen, I stopped debug at line 294.In lines 287 and 289 GPIOD->MODER and memory adress 0x4800 0C00 should be set to some value unequal ze...

0690X0000060A0zQAE.png

External loader in ST utility

Posted on March 15, 2018 at 17:16I am trying to create a custom external loader for the flash chip used in my product. I have looked the example projects in IAR and created myown. I modified the Loader_src.c and Dev_Inf.c file according to my flash ...

stm32Fxxx ICT using JTAG

Posted on March 15, 2018 at 16:20To begin, this is a board TEST question rather than a design question: Has anyone successfully generated digital In-Circuit Test vectors for the STM32F4xx families using the Keysight 3070 or Teradyne scan tools? I su...

NUCLEO-H743ZI LWIP using STM32cubeMX?

Posted on November 06, 2017 at 11:11Hi,  I generated a simple LWIP/UDP project for the NUCLEO-H743ZI using the STM32cubeMX. But the function HAL_ETH_Transmit(&heth, &TxConfig, 0); returns with DMA error .  My board works using the example from the S...

Asantos by Senior
  • 1359 Views
  • 4 replies
  • 0 kudos

Reading variable length strings from a usart with DMA

Posted on October 05, 2017 at 22:44 I need to read variable length strings from a usart. The strings may be the result of local programming or not. I'm using the HAL DMA receive driver under FreeRTOS. I've found that the following approach works:...

Second I2C bus generating 60 Hz square wave at SCL

Posted on March 15, 2018 at 14:51I have successfully implemented an initial I2C bus (I2C1) in my custom board design (using STM32F405).  I then added a second I2C bus (I2C2) to my design and have initiated it and set it up identical to I2C1.  The fi...

Eric P by Associate
  • 852 Views
  • 1 replies
  • 0 kudos