User Activity

Posted on November 20, 2017 at 13:56HiI'am trying to migrate existing SPL based flash erase and program code to LL. Some flash routine are part of the xxx_ll_system driver but I am missing the erase and program routines such as the FLASH_ProgramWord...
Posted on October 18, 2017 at 14:50HiI'm using I2C1 periphery of a STM32F205 device in master mode. The firmware is based on the HAL V1.2.1 driver with interrupt approach. Three slaves are attached to the bus and 7bit address mode is used. I'm able ...
Posted on January 06, 2017 at 15:42We use the STM32F100VC for one of our projects. We were able to order devices marked as STM32F100VCTB (Revision A) and the STM32F100VCT (Revision X). Based on the ordering information of the device the letter 'B' s...
Posted on August 26, 2013 at 09:41Hello I tried to migrate a working SPI master from a STMF20x device to the STM32F37x device. The SPI master should write and read 8bit data to some SPI memory devices (EEPROM or flash) by using DMA. Attached is the ...
Posted on March 11, 2013 at 14:13Hi We figured out some ADC channel miss match on STM32F100C8 device, which we couldn't explane. We use the following test setup: - ADC1_IN0 (PA0) to ADC1_IN3 (PA3) are used. - Regular group scan mode with DMA is used...
Kudos from