Dear All,Please consider STM32F407. I tried to configured its three ADCs: ADC1 and ADC2 in dual intereleved and ADC3 in independent mode using CubeMX. BUT it is impossibe the job using that. Is it possible to moddify the CubeMX's generated code to wo...
Dear All,I am confused with using LTDC working with ili9341 in the discovery f429.LTDC is an tft controller. so I expect there is not required and extra external controller.what is the issue?Best regards, Ras
Posted on November 21, 2017 at 20:54dear All,what is the probable reason of HAL_I2C_Master_Transmit() transmits only address?regards,Rasool#i2c #stm32f4 #master-trasnmitter
Posted on November 20, 2017 at 20:16dear ST Community,i am trying to talk to a smart battery through SMBus as bellow:to initialize: an I2C of the STM32F407 as SMBus.to transmit battery address ( slave )to acknowledge from itbut the command doesn't b...