STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F407VGXT DIscovery GPIO state at start_up

Posted on April 20, 2018 at 14:47Hi all, I'm using stm32f4 discovery with HAL drivers to realize a Synchronous BOOST DCDC.When the system is turn on, the gpio PE8 and PE9 configured as PWM pins of TIM1,(in particular PWMOUT_CH1 & PWMOUT_CH1N) goes i...

SPBTLE-RF in STM32L4 Discovery kit IoT node

Posted on April 20, 2018 at 16:04Hi!!Can anyone give me a SPBTLE-RF module tutorial or some sample code for a STM32L4 Discovery kit IoT nodeCheers.#spbtle-rf #stm32l4-discovery-kit-iot-node #spbtle-rf-in-stm32l4-discovery-kit-iot-node

Resolved! use PH3 pin as GPIO instead of BOOT0

Posted on April 18, 2018 at 14:11Hello all,In STM32L432KB, I want to use PH3 pin as GPIO, instead of BOOT0 without affecting its boot sequence.How should I achieve it ?

Resolved! How to do a byte program on my STM32L4R5 platform ?

Posted on April 20, 2018 at 05:19I didn't find a way to do a byte program on my STM32L4 , there is a doubleword program exist in the stm32l4xx_hal_flash.c file.How can i do that , read the doubleword out first and modify one byte and do a doubleword...

fema by Associate III
  • 1870 Views
  • 5 replies
  • 1 kudos

write to flash mem stm32f429

Posted on April 19, 2018 at 11:11hello evrybody, i can write to stm32f103c8/cb with no prblms using hal functions ,but now i need to write to stm32f429ZI nucleo cart , but no success some times i can what i wrote by coinsidence but this is very stra...

ETM not working on stm32f7

Posted on February 24, 2016 at 11:29 hi, i am using stm32f7 and for debugging ulink pro, i have tried to enable ETM but not succedded. the connector i am using is, where traceD0-D3 are PE3-PE6. th...

0690X000006052bQAA.png 0690X00000605MLQAY.png
bilal by Associate II
  • 1668 Views
  • 1 replies
  • 0 kudos

STM32F4 ETM Trace configuration problem

Posted on March 13, 2017 at 11:40Hi,I'm using ULINKpro and Keil uVision 5.23.0.0 as debugger.I can't make ETM Trace (sync mode, 4-bit data) works properly on a STM32F427ZG with a core clock of 168MHz.I tried to lower the core clock working frequency...

0690X00000603m2QAA.jpg 0690X00000603b7QAA.jpg 0690X00000603m7QAA.jpg

Resolved! Detecting long button press on STM32F3

Posted on April 20, 2018 at 13:03Hi,I'm trying to detect a long button press on an STM32F3.I have a push button connected to a GPIO on the STM32F3 configured with an external interrupt request (EXTI9_5_IRQn). The interrupt handler (HAL_GPIO_EXTI_IRQ...