2017-12-27 9:52 AM
All of the FATFs examples (and indeed, CubeMX) appear to be geared toward the STM32F series chips when using FatFS. I want to use the STM32L433, insofar as I have a lot of my application already written for that device. Now they want to add a file system and SD card...
Am I 'spitting into the wind' trying to get a L series chip to work with this? Does it not have enough horsepower to do the job? I'll be writing something on the order of 35 bytes at a 720 samples/second rate. Will this keep up with DMA?
Writing to another device is possible, but the ultra-lower power consumption is one of the attractions to this chip.Thanks,
John
2017-12-27 11:18 AM
The L475 has an MMC/SDIO interface that should work, the others likely workable with SPI
I would tend to avoid multiple small writes, you should accumulate data and write in multiples of 512 bytes.
2017-12-27 11:44 AM
The Discovery STM32L496 has microSD card demo, so I would probably look into the example code and adapt if they share the same reference manual (the same bag of design IPs)