STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART communication not working properly

Posted on April 20, 2018 at 12:29Hello, I am trying to cummunicate with device throught UART, but communication is not working reliably. I am trying to read data continuosly by transmitting request in infinite loop, but I receive incomplete or curru...

Noisy ADC Channels and UART issues

Posted on April 24, 2018 at 12:43Hello,I have a Nucleo STM32L476RG board. I am using it to read time varying ADC values from 3 channels of ADC1 (PC_0,PC_1,PC_2) and print them as a single comma separated string. Eg. 100,134,130.Here are a few detail...

0690X0000060AkwQAE.png 0690X0000060Al1QAE.png 0690X0000060Al6QAE.png 0690X0000060AhUQAU.png

STM32L4 uart wrong init order

Posted on April 24, 2018 at 11:01Hi Dev Team,I found a bug in the HAL_UART_Init function provided by the above library. The advanced features are applied with UART_AdvFeatureConfig after the standard features are applied with UART_SetConfig.I config...

HAL_UART_IRQHandler() calls UART_Receive_IT() on error in STM32CubeF1 Firmware Package V1.6.0 / 17-May-2017

Posted on April 24, 2018 at 10:41Configure UART with HAL_UART_Init() with some baudrate 'X' Start receiving with HAL_UART_Receive_IT(Size = 1) Send any frame with baudrate different than 'X'catch HAL_UART_RxCpltCallback() followed by HAL_UART_ErrorC...

Different binary sizes when building

Posted on April 23, 2018 at 19:14HI there,This isn't a question related to ST products, but I'm just curious about something that I started noticing. I am developing my project on Atollic TrueSTUDIO, and when I build the project using the CDT Manged...

Getting Issue in low power modes.

Posted on April 24, 2018 at 09:19Hi ,I am working on Low power modes for STM32L053C8.My MCU go in STOP and SLEEP Mode,but not coming out from the STOP and sleep mode.I am using STM32L053 discovery board.have confiigure one button as a wake up interr...

Resolved! i am working on stm32f030c6t6 microcontroller.

Posted on April 23, 2018 at 10:35Hi all,I am working on stm32f030c6t6 microcontroller. I want to use tim3_ch1 as pwm output. datasheet says that tim3_ch1 alternate function is available at two pins PA6 and PB4.I am not able to find that which pin de...

sanju by Senior
  • 2734 Views
  • 6 replies
  • 0 kudos