STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! HSE RDY high without HSE clock ?

Posted on April 29, 2018 at 13:55I am using the Nucleo-64 board F401RE, as the name suggest comes with STM32F401RE.The board doesn't have an external clock (X3 mentioned on the board) and still the HSE RDY register gets enabled  , which is actually ...

STM32L496 with a external 6 channel parallel ADC.

Posted on April 13, 2018 at 10:39I am firmware engineer. But I am a beginner for ST.I try to get 6 channel ADC 16bit data in high spped by DMA.Now, I have a nucleo-L496ZG board and a TI ADS8364 ADC board.- STM32L496ZG (with FMC)- TI ADS8365 (6 Chann...

STM32F405 RTC counting more than 24h!

Posted on April 27, 2018 at 15:47The RTC continues to count after 23:59:59, just changes the day at 39:59:59, what's the problem?I use HAL Library.RTC Output:2018-04-06 weak5, 23:59:572018-04-06 weak5, 23:59:582018-04-06 weak5, 23:59:592018-04-06 we...

Resolved! timer reset counter on falling edge

Posted on April 28, 2018 at 01:37 Hey everyone, I can not seem to get this right and any help would really be appreciated! I'm using a stm32f722ze I have a counter that toggles it's output on every 10th rising clock edge of an external clock ...

0690X00000604cwQAA.jpg 0690X00000604RRQAY.jpg 0690X00000604dVQAQ.jpg
con3 by Senior
  • 1578 Views
  • 2 replies
  • 0 kudos

STM32F103 Maximum input Frequency

Posted on April 28, 2018 at 19:09I use STM32F103 how much is the maximum input maximum encoder frequency. For example if the possible i reading the 20 KHz. I use the TIMER4 encoder mode but i not read the up the 2 KHz. How much is the maximum freque...

Resolved! STM32F767 Nucleo144 - Default clock frequency

Posted on April 28, 2018 at 12:54Hi,what is the default system clock frequency (previous that all clock configuration take place) on the development board 'STM32F767 Nucleo-144'?Where I can find this information?Thank you for the answer.