cancel
Showing results for 
Search instead for 
Did you mean: 

Any possibility: Get ADC input on PA9

Patrick Morwald
Associate II
Posted on January 17, 2018 at 14:42

Hi,

this might be a stupid question because datasheet says there is no ADC in pin PA9 on a STM32F407VGT, 

so what i am probably asking is if there is any way of working around this / finding a hack?

Background is that we have an already produced PCB where the pin PA9 is routed to an analog sensor output and i need to read the analog signal somehow.

Regards,

Patrick  

#pin-configuration #adc #stm32f4
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
waclawek.jan
Super User
Posted on January 17, 2018 at 15:07

if there is any way of working around this

No.

JW

toby2
Senior
Posted on January 17, 2018 at 15:20

Not in SW, as Jan said.

But if it is a QFP package it might be possible to bridge to an unused pin which is an ADC input?

Patrick Morwald
Associate II
Posted on January 17, 2018 at 15:55

Thanks for the answer. Ok i will try to bridge to another pin.