STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F427 does not boot after power on

Posted on April 26, 2018 at 17:16Hello,i  am using a design with a STM32F427  100pin package, and notice after leaving the board unpowered for several hours if i power up again, the software its not starting.If i retry the restat the power it will s...

Bogdan by Senior
  • 4013 Views
  • 10 replies
  • 0 kudos

linker script help: What is meant by >RAM_D1 AT> FLASH

Posted on April 28, 2018 at 02:30This follows the .data {....} section.  I think I understand the first part >RAM_D1 meaning the data sections start in the RAM_D1 memory who's origin is 0x240000000 in my case, but what does the AT> Flash do?  My gue...

Erasing chip after Level 2 protection

Posted on April 27, 2018 at 15:00Hi,  I am testing a Nucleo-64 stmL07xxx board and playing around with the protection parts.  After I added my application I set Level 2 protection to prevent read/erase and program of processor. It says its irreversa...

STM32F4 - fastest IIR biquad impelementation in Assembler

Posted on April 27, 2018 at 12:07Hi,I need the fastest implementation of a biquad IIR filter for STM32F4 in assembler. I have to run more than 60 filters at 48kHz. My current best time are 24 cycles per filter with TDF2 (17 at STM32F7).The order of ...

koster by Associate III
  • 1649 Views
  • 2 replies
  • 0 kudos

Using STLink Utility to protect bootloader

Posted on April 27, 2018 at 16:40Hi  I have been looking on the forum and web regarding flash memory protection,writing etc...  I basically want to write a custom bootoader and have its memory , 1st page, write protected to prevent any overwriting. ...

How to access PMOD ENCoder using STM32L475

Posted on April 27, 2018 at 15:52Dear all,I need example program how to access PMOD ENCoder using STM32L475.https://reference.digilentinc.com/reference/pmod/pmodenc/start&sharpexample_projects Thank you very much in advance.warmest regards,suryadi#p...

cubef4 STM32F4-Discovery dac example problem?

Posted on April 27, 2018 at 15:04hii  want use DAC_SignalsGeneration example for Making waveforms in my stm32f407 discovery eval board i redefineconst uint8_t aEscalator8bit[6] = {0x0, 0x33, 0x66, 0x99, 0xCC, 0xFF};toconst uint16_t aEscalator16bit[1...

Resolved! STM32F4 power measurement firmware

Posted on April 21, 2018 at 15:36Where can i get the power measurement firmware mentioned in this application note by STAN4365 Using STM32F4 MCU power modes with best dynamic efficiencyThe project used in the AN is coremark based . Can i get this pr...

n.serina by Associate III
  • 1774 Views
  • 4 replies
  • 0 kudos