STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI Slave Register Reset

Posted on April 16, 2018 at 18:37I have an issue with the SPI slave interface in the ST32ML151. Occasionally, the SPI slave get an extra clock from outside, either because noise or a reset at the master side. I know when this happens. Is there a way...

Firmware Over The Air upgrade issue

Posted on April 28, 2018 at 21:00I have developed a Firmware upgrade Over The Air (FOTA) mechanism for my custom F7 board that seems to work properly, but hard faults during the subsequent reboot process of the main application.Thanks to Clive1's su...

0690X0000060AoPQAU.png 0690X0000060AoeQAE.png 0690X0000060ApZQAU.png

Receive variable length buffer on UART (Interrupt)

Posted on April 30, 2018 at 18:32 Hello, in my project I have to receive commands from the serial port (UART), these commands are of variable length and end with carriage return (\r). what I would like to do is generate an interrut when the \...

Select ADC channel to convert

Posted on April 30, 2018 at 18:16 hi, I have a problem using an ADC of a STM32L4 In my project I have to sample 5 analogue channels with an ADC. I've configured everything with STM32CubeMX and want to use it in polling mode. I have seen examples ...

STM32CubeMX MCU package for STM32F1, LSE & RTC problems

Posted on April 14, 2018 at 13:06Using:Truestudio for STM32 v9.0.0.0STM32CubeMX v4.25.0 with STM32CubeF1 Firmware Package V1.6.1uC STM32F103RBLL_drivers onlyLL_Code generated for the STM32F1 family by STM32CubeMx  seems to fail to configure the LSE ...

Willunen by Associate III
  • 1268 Views
  • 2 replies
  • 0 kudos

How to configure External clock in stm32f103 ????

Posted on April 30, 2018 at 10:38Hi,I'm using STM32F103 board, I connected 8Mhz Quartz crystal to pin PD0 and PD1 ( i.e. OSCIN and OSCOUT). But the oscillator is  not working, even I gave supply to Vbat pin.Is their any configuration required I soft...

FatFs - SDMMC - STM32H7

Posted on February 21, 2018 at 16:20Hi,I have the problem that many of us have as seen on the number of post on the forum. Unfortunatly for me nobody have the same issue as i have!Let s point out first what i'm trying to do.I'm on a small project of...