cancel
Showing results for 
Search instead for 
Did you mean: 

External Interrupt via GPIO cannot be triggered after waking up from STOP mode

Thomas Hoppe
Associate III
Posted on January 17, 2018 at 14:44

I have a problem with a project based on an STM32L051. I want to use the stop mode and wake up on an external (GPIO based) IRQ. This all works great but after the MCU woke up, no other IRQs seem to work. I have a very simple IRQ handler which just outputs some debug info for now. Naturally I do hal-initialize again after I woke up. Also the whole thing works when I use stand-by mode instead of stop mode. I tried to enable the related IRQ via HAL_NVIC_EnableIRQ(EXTI0_1_IRQn); explicitly but it did not help. Any idea what could be missing?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0