STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

flashing stm32F303 based custom board

Posted on May 03, 2018 at 23:36Hello,I am making a custom board based on STM32F3 discovery board. My custom board is an exact copy of the discovery board with additional sensor components. I can easily program STM32F3 board as st-link is already bui...

STM32L4 register setting

Posted on May 03, 2018 at 19:43I'm trying to program STM32L4-discovery board using the registers of ST32L4 only. I wanted to modify flash latency and see if the register value really changes by using gdb. However, it turned out that the following si...

M. Jeong by Associate II
  • 813 Views
  • 2 replies
  • 0 kudos

Cubemx 4.25 STM32F767 EXTI problem

Posted on April 03, 2018 at 20:44I've configured a number of pins on the 767 as EXTI but there is no option in NVIC to enable the interrupts and no code generated. The pins are correctly identified in  the GPIO configuration tab.Moreover, the exampl...

Using ll_sdmmc.c with eMMC

Posted on April 25, 2018 at 16:40Hi,I�m working on a project with the STM32L4 on a custom board. We want to access a eMMC to store acquired data. First, we used the HAL_sd.c library, but since it�s not compatible with eMMC, we now want to use the lo...

Maxim H by Associate
  • 1107 Views
  • 1 replies
  • 0 kudos

How to get SiLabs CP2102N working as a USB device?

Posted on May 03, 2018 at 18:03Hello,I'm working on a board based on STM32F427 MCU. The board is implemented as a USB Host.I'm trying to get SiLabs' CP2102N working as a USB device. I understand I'll need to change the driver to make it work. Have a...

Pilot B by Associate II
  • 669 Views
  • 0 replies
  • 0 kudos

ENABLING STPM32 COMMUNICATION...!!!!!

Posted on March 26, 2018 at 07:10I am using STPM32 with STM32F4 microcontroller series. We are using UART communication. When we trying to reset the whole framework the controller only receives 0 values for 48th register. When we are trying to set t...

Problem with STM32F746 : EXTI15_10_IRQ is constantly fired

Posted on March 29, 2018 at 13:55Hi, today I have observed and solved a problem when I started to develop my simple program for NUCLEO-F746ZG. A problem  was following: EXTI15_10_IRQHandler interrupt fired always - regardless of my changes in progra...

juozas by Associate III
  • 1252 Views
  • 2 replies
  • 0 kudos