Comparator in STM32F373?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-01-19 1:34 AM
Posted on January 19, 2018 at 10:34
Hello i have any question about Comp in STM32F3
1. W
hat is the p
ropagation delay for low overdrive, for example 5mV? In DS is only for 100mV. For High speed mode.2. W
hat is the output current for Low and high level on output commparatar?
3. What is the large-signal differential voltage amplification?
4. If is used internal DAC for driving one comparator input, can be used DAC without buffer?
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0