STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7 GPIO TOGLE MAX FREQUENCY

Posted on May 07, 2018 at 14:08With STM32F765 and MDK-ARM compiler ( O3 and compile for SPEED I was able to achieve 108Mhz on output pin, performing while loop ( just main() and all interrupt disabled ) .Now with STM32H743 with same compiler and sam...

TIMPRE HCLK multiplier in F413

Posted on May 17, 2018 at 11:08In RM0430 rev 7 section 6.2 it is stated that when TIMPRE is set and APB prescaler is 1 or 2 then the timer clock is HCLK.And when APB prescaler is > 2 then the timer clocks are HCLK * 4.This is different to the F446 w...

Bootloader unavalability due to Pin HW state

Posted on May 17, 2018 at 14:17Hello!currently looking into bootloader modes and working with the STM32F7.while going over the AN2606 document (STM32 microcontroller system memory boot mode)i noticed an issue - 'Bootloader unavailability on STM32F10...

yuri CH by Senior
  • 1054 Views
  • 1 replies
  • 0 kudos

Timer Compare Output - How to rearm timer

Posted on May 16, 2018 at 10:08Board/Processor : STM32L476RG-NucleoExample code from: STM32Cube_FW_L4_V1.10.0ARM IAR compiler V8.I can successfully build and run the TIM_OCActive / TIM_OCInactive examples on the above board, they produce the require...

Rob Peck by Associate
  • 2057 Views
  • 4 replies
  • 0 kudos

STM32F746 Discovery VBAT

Posted on April 26, 2017 at 19:03Why the big featured STM32F746 Discovery Lacks in External VBAT pins This makes the board completely unusable for backup test and RTC time keep upThe designer had concentrated only on big features like LCD, SDRAM, FL...

I think that I have found problem in HAL

Posted on May 14, 2018 at 14:02 Dear Sirs/Madams, I am developing firmware for our device with your STM32F745 microcontroller. I use STM32F7 HAL. I also use STM32CubeMX (v.4.0) with STM32Cube MCU Package for STM32F7 Series (v.1.0). I use EWAR...

uint32_t Buttons_GetState (void) explanation?

Posted on May 16, 2018 at 22:42Hi All,Just saw the BSP for buttons on Keil, came across this, can anyone explain how this actually works when one presses the button.Apparently if one was supposed to press button say at pin 13 in this case, GPIOC->ID...