User Activity

Posted on January 24, 2018 at 19:23Hi All       I am trying to get the TIM16 to work in output compare mode especially generate a PWM signal on channel 1. I am using the LL libraries of STM32L4xxx to do the job. I am using NUCLEO L432KC board and pr...
Posted on October 20, 2017 at 22:51Hi    I am using STM32L431xx Timer3 and CC3 (compare mode ) on channel 3 and i want to trigger (ADC1  channel 1) and (DMA 1 and channel 1 ) to do collection of samples triggered on the timer edge. The timer works p...
Posted on October 03, 2017 at 15:42Hi     I hooked up two STM32L432 nucleo boards in master-salve mode of SPI. I am setting up DMA and SPI with 8 bit (BYTE) boundary and data width.  If I set the FRXTH threshold  for SPI  as LL_SPI_RX_FIFO_TH_HALF t...
Posted on September 29, 2017 at 21:08Hi   I want to use only the STM32L432 LL drivers by  defining the label USE_FULL_LL_DRIVER. Does anyone have example codes for the blocks like SPI using only drivers and not the HAL?.... Please help.RegardsBala
Posted on September 09, 2017 at 00:06Hi    I am trying to write my own HAL for STM32L43x deivce basically on the neucleo board that I purchased. I wonder if any of you guys know where I can just download the peripheral drivers... I know STM provide ...
Kudos from