2018-01-30 6:53 AM
hello friends i recently got an stm32l4 I just go past the led blink i am trying my hands on interrupts I am trying to configure a falling edge triggered interrupt on A0 and PC15 so far works fine for GPIOA but the interrupt for GPIOC15
is not working
I have enabled pull up on the pin but when i drive it low it doesnt trigger the interrupt during the debug i know cause the counter in the ISR is not incrementing
does anyone know why my c code is below i am using keil ide thank you
#include 'stm32l433xx.h'
extern int cnt,j;
void EXTI0_IRQHandler(void){if (!(GPIOA->IDR & (1<<0)) )
{ if(!(cnt%2)) GPIOC->ODR =~(1<<4); else GPIOC->ODR|= (1<<4); cnt++; }//Clear the EXTI pending bits
NVIC_ClearPendingIRQ(EXTI3_IRQn); EXTI->PR1 |=(1<<0);}void EXTI15_IRQHandler(void){ j++; NVIC_ClearPendingIRQ(EXTI15_10_IRQn); //Clear the EXTI pending bits EXTI->PR1 |=(1<<15);}void Config_IO(void) { RCC->AHB2ENR |= RCC_AHB2ENR_GPIOBEN; RCC->AHB2ENR |= RCC_AHB2ENR_GPIOCEN; RCC->AHB2ENR |= RCC_AHB2ENR_GPIOAEN; GPIOA->MODER &=~(1<<0); //input mode for A0 GPIOA->MODER &=~(1<<1); GPIOA->PUPDR |= (1<<0); //pull up on A0 GPIOA->PUPDR &=~(1<<1); GPIOA->OSPEEDR |=(1<<0); //input mode for A0 GPIOA->OSPEEDR |=(1<<1); GPIOA ->OTYPER &=~(1<<0); GPIOB ->MODER &= ~(GPIO_MODER_MODER13_0); // set GPIO 13 as general purpose input GPIOB ->MODER &= ~(GPIO_MODER_MODER13_1); GPIOB ->PUPDR &= ~(1<<27); //10000000000 Pull up RB13 GPIOB ->PUPDR |= (1<<26); GPIOC ->MODER |= GPIO_MODER_MODE12_0; ///set GPIO13 as general output GPIOC ->MODER &= ~(GPIO_MODER_MODE12_1); GPIOC ->OTYPER &= ~(GPIO_OTYPER_OT_12); ///push pull output type for GPIOC12 GPIOC ->OSPEEDR |= (GPIO_OSPEEDER_OSPEEDR12_0); // high speed for GPPIOC12 GPIOC ->OSPEEDR |= (GPIO_OSPEEDER_OSPEEDR12_1); GPIOC ->PUPDR &= ~(GPIO_PUPDR_PUPDR12); //NO PULL UP*/ GPIOC ->MODER |= (1<<8); //PC4 output mode GPIOC ->MODER &= ~(1<<9); GPIOC ->OTYPER |= (1<<4); //open drain on PC4 GPIOC ->OSPEEDR |= (1<<8); //PC4 high speed GPIOC ->OSPEEDR |= (1<<9); GPIOC ->PUPDR &=~(0<<8); GPIOC ->PUPDR &=~(0<<9); GPIOB->MODER &=~(1<<30); //input mode for B15 GPIOB->MODER &=~(1<<31); GPIOB ->PUPDR &= ~(1<<31); //10000000000 Pull up B15 GPIOB ->PUPDR |= (1<<30); GPIOB ->OTYPER &= ~(1<<15); ///push pull output type for GPIOB15 GPIOB ->OSPEEDR &= ~ (1<<30); //PB15 high speed GPIOB ->OSPEEDR |= (1<<31); } void Config_Interrupt(void){ SYSCFG->EXTICR[0] &= SYSCFG_EXTICR1_EXTI0_PA; SYSCFG->EXTICR[3] = SYSCFG_EXTICR4_EXTI15_PB ; EXTI->IMR1 |= (1<<0); EXTI->IMR1 |= (1<<15);EXTI->EMR1 |=(1<<0); //interrupt source is unmaskrd
EXTI->EMR1 |=(1<<15); //Unmask interrupt line 15 EXTI->FTSR1 |= (1<<0); //falling edge line 1 EXTI->FTSR1 |= (1<<15); //falling edge line 15 __enable_irq(); //enable interrupt NVIC_SetPriority(EXTI0_IRQn,4); //Set priority NVIC_SetPriority(EXTI15_10_IRQn,4); NVIC_ClearPendingIRQ(EXTI0_IRQn); //clear pending NVIC_ClearPendingIRQ(EXTI15_10_IRQn); NVIC_EnableIRQ(EXTI0_IRQn); ///enable interrupt NVIC_EnableIRQ(EXTI15_10_IRQn); }void Config_IO(void);
void Config_Interrupt(void);int cnt,i,j;int main()
{ Config_IO(); Config_Interrupt(); while (1) { GPIOC->ODR|= (1<<12); for(i=0;i<100;i++); GPIOC->ODR&= ~(1<<12); for(i=0;i<100;i++); } return 0; }Solved! Go to Solution.
2018-01-30 8:14 AM
void EXTI15_10_IRQHandler(void)
2018-01-30 8:14 AM
void EXTI15_10_IRQHandler(void)
2018-01-30 9:03 AM
Thank you waclawek i i modified the code like you suggested i have changed the IRQ handler to
void EXTI15
_10_IRQHandler(void)
and i setRCC_APB2ENR.SYSCFGEN in my config_io fucntion line 40
the interrupt is still not triggering i tried another pin PB3 but so far thats not working either the code looks like this now
#include 'stm32l433xx.h'
extern int cnt,j;
void EXTI0_IRQHandler(void){if (!(GPIOA->IDR & (1<<0)) )
{ if(!(cnt%2)) GPIOC->ODR =~(1<<4); else GPIOC->ODR|= (1<<4); cnt++; }//Clear the EXTI pending bits
NVIC_ClearPendingIRQ(EXTI3_IRQn); EXTI->PR1 |=(1<<0);}void EXTI15_10_IRQHandler(void){ cnt++; j++; NVIC_ClearPendingIRQ(EXTI15_10_IRQn); //Clear the EXTI pending bits EXTI->PR1 |=(1<<15);}void EXTI1_IRQHandler(void)
{ cnt++; j++; NVIC_ClearPendingIRQ(EXTI1_IRQn); //Clear the EXTI pending bits EXTI->PR1 |=(1<<3);}void Config_IO(void) { RCC->APB2ENR |=(1<<0); //SYSCFG ENABLE RCC->AHB2ENR |= RCC_AHB2ENR_GPIOBEN; RCC->AHB2ENR |= RCC_AHB2ENR_GPIOCEN; RCC->AHB2ENR |= RCC_AHB2ENR_GPIOAEN; GPIOA->MODER &=~(1<<0); //input mode for A0 GPIOA->MODER &=~(1<<1); GPIOA->PUPDR |= (1<<0); //pull up on A0 GPIOA->PUPDR &=~(1<<1); GPIOA->OSPEEDR |=(1<<0); //input mode for A0 GPIOA->OSPEEDR |=(1<<1); GPIOA ->OTYPER &=~(1<<0); GPIOB ->MODER &= ~(GPIO_MODER_MODER13_0); // set GPIO 13 as general purpose input GPIOB ->MODER &= ~(GPIO_MODER_MODER13_1); GPIOB ->PUPDR &= ~(1<<27); //10000000000 Pull up RB13 GPIOB ->PUPDR |= (1<<26); GPIOC ->MODER |= GPIO_MODER_MODE12_0; ///set GPIO13 as general output GPIOC ->MODER &= ~(GPIO_MODER_MODE12_1); GPIOC ->OTYPER &= ~(GPIO_OTYPER_OT_12); ///push pull output type for GPIOC12 GPIOC ->OSPEEDR |= (GPIO_OSPEEDER_OSPEEDR12_0); // high speed for GPPIOC12 GPIOC ->OSPEEDR |= (GPIO_OSPEEDER_OSPEEDR12_1); GPIOC ->PUPDR &= ~(GPIO_PUPDR_PUPDR12); //NO PULL UP*/ GPIOC ->MODER |= (1<<8); //PC4 output mode GPIOC ->MODER &= ~(1<<9); GPIOC ->OTYPER |= (1<<4); //open drain on PC4 GPIOC ->OSPEEDR |= (1<<8); //PC4 high speed GPIOC ->OSPEEDR |= (1<<9); GPIOC ->PUPDR &=~(0<<8); GPIOC ->PUPDR &=~(0<<9); GPIOB->MODER &=~(1<<30); //input mode for B15 GPIOB->MODER &=~(1<<31); GPIOB ->PUPDR &= ~(1<<31); //10000000000 Pull up B15 GPIOB ->PUPDR |= (1<<30); GPIOB ->OTYPER &= ~(1<<15); ///push pull output type for GPIOB15 GPIOB ->OSPEEDR |= (1<<30); //PB15 high speed GPIOB ->OSPEEDR |= (1<<31); GPIOB->MODER &=~(1<<6); //input mode for B3 GPIOB->MODER &=~(1<<7); GPIOB ->PUPDR &= ~(1<<7); //10000000000 Pull up B3 GPIOB ->PUPDR |= (1<<6); GPIOB ->OTYPER &= ~(1<<3); ///push pull output type for GPIOB3 GPIOB ->OSPEEDR |= (1<<6); //PB15 high speed GPIOB ->OSPEEDR |= (1<<7); } void Config_Interrupt(void) { SYSCFG->EXTICR[0] &= SYSCFG_EXTICR1_EXTI0_PA; SYSCFG->EXTICR[1] = SYSCFG_EXTICR4_EXTI15_PB ; SYSCFG->EXTICR[1] = SYSCFG_EXTICR1_EXTI1_PB ; EXTI->IMR1 |= (1<<0); EXTI->IMR1 |= (1<<15); EXTI->IMR1 |= (1<<3);EXTI->EMR1 |=(1<<0); //interrupt source is unmaskrd
EXTI->EMR1 |=(1<<15); //Unmask interrupt line 15 EXTI->EMR1 |=(1<<3); EXTI->FTSR1 |= (1<<0); //falling edge line 1 EXTI->FTSR1 |= (1<<15); //falling edge line 15 EXTI->FTSR1 |= (1<<3); __enable_irq(); //enable interrupt NVIC_SetPriority(EXTI0_IRQn,4); //Set priority NVIC_SetPriority(EXTI15_10_IRQn,4); NVIC_SetPriority(EXTI1_IRQn,4); NVIC_ClearPendingIRQ(EXTI0_IRQn); //clear pending NVIC_ClearPendingIRQ(EXTI15_10_IRQn); NVIC_ClearPendingIRQ(EXTI1_IRQn); NVIC_EnableIRQ(EXTI0_IRQn); ///enable interrupt NVIC_EnableIRQ(EXTI15_10_IRQn); NVIC_EnableIRQ(EXTI3_IRQn); }#include 'stm32l433xx.h'
extern int cnt,j;
void EXTI0_IRQHandler(void){if (!(GPIOA->IDR & (1<<0)) )
{ if(!(cnt%2)) GPIOC->ODR =~(1<<4); else GPIOC->ODR|= (1<<4); cnt++; }//Clear the EXTI pending bits
NVIC_ClearPendingIRQ(EXTI3_IRQn); EXTI->PR1 |=(1<<0);}void EXTI15_10_IRQHandler(void){ cnt++; j++; NVIC_ClearPendingIRQ(EXTI15_10_IRQn); //Clear the EXTI pending bits EXTI->PR1 |=(1<<15);}void EXTI1_IRQHandler(void)
{ cnt++; j++; NVIC_ClearPendingIRQ(EXTI1_IRQn); //Clear the EXTI pending bits EXTI->PR1 |=(1<<3);}#include 'stm32l433xx.h'
void Config_IO(void);
void Config_Interrupt(void);int cnt,i,j;int main()
{ Config_IO(); Config_Interrupt(); while (1) { GPIOC->ODR|= (1<<12); for(i=0;i<100;i++); GPIOC->ODR&= ~(1<<12); for(i=0;i<100;i++); } return 0; }2018-01-30 9:25 AM
and set RCC_APB2ENR.SYSCFGEN
2018-01-31 2:24 AM
Read back the SYSCFG and GPIO registers and check if they contain what you expect.
Look at the actual vector table (in binary, or better in disassembled binary) if the address at expected position points to the actual interrupt routine.
JW
2018-01-31 3:11 AM
the flow looks generally right. two suggestions:
1) simplify your code to a minimalist framework.
2) be consistent: if you are using pin13 as the exti, program your code so it consistently use that pin. I typically define a mask and use that mask throughout my code so if I want to move to a different pin, I can. your code has tons of hard-coded numbers that are inconsistent from one place to another, making it hard to track.